2022-08-10 07:42 AM
Here is the github link of the flutter layer:
https://github.com/meta-flutter/meta-flutter
ERROR: flutter-engine-git-r0 do_install: ExpansionError('do_install', "\n install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/so.unstripped/libflutter_engine.so \\\n /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/lib/libflutter_engine.so\n\n if ${@bb.utils.contains('PACKAGECONFIG', 'desktop-embeddings', 'true', 'false', d)}; then\n install -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/so.unstripped/libflutter_linux_gtk.so /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/lib\n fi\n\n install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/flutter_embedder.h \\\n /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/include/flutter_embedder.h\n\n install -D -m0644 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/icudtl.dat \\\n /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/icudtl.dat\n\n # create SDK\n install -D -m0755 /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/out/linux_release_arm/clang_x64/gen_snapshot \\\n /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/clang_x64/gen_snapshot\n\n cd /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/src/flutter\n echo `git rev-parse HEAD` > /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/engine.version\n echo ${FLUTTER_ENGINE_REPO_URL} >> /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/engine.version\n echo ${@get_flutter_sdk_version(d)} >> /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image/usr/share/flutter/sdk/flutter_sdk.version\n\n cd /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/image//usr/share/flutter\n zip -r engine_sdk.zip sdk\n rm -rf sdk\n", URLError(gaierror(-3, 'Temporary failure in name resolution')))
ERROR: Logfile of failure stored in: /home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/flutter-engine/git-r0/temp/log.do_install.3657615
Log data follows:
| DEBUG: Executing python function extend_recipe_sysroot
| NOTE: Direct dependencies are ['/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-graphics/fontconfig/fontconfig_2.13.1.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/meta-flutter/recipes-devtools/depot-tools/depot-tools-native_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-extended/zip/zip_3.0.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-support/curl/curl_7.82.0.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/quilt/quilt-native_0.67.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/pkgconfig/pkgconfig_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/python/python3_3.10.4.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-core/glibc/glibc_2.35.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/clang-cross_git.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/compiler-rt_git.bb:do_populate_sysroot', '/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/meta-clang/recipes-devtools/clang/libcxx_git.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-support/ca-certificates/ca-certificates_20211016.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-devtools/patch/patch_2.7.6.bb:do_populate_sysroot', 'virtual:native:/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/layers/openembedded-core/meta/recipes-extended/pbzip2/pbzip2_1.1.13.bb:do_populate_sysroot']
| NOTE: Installed into sysroot: []
| NOTE: Skipping as already exists in sysroot: ['fontconfig', 'depot-tools-native', 'zip-native', 'curl-native', 'quilt-native', 'pkgconfig-native', 'pseudo-native', 'python3-native', 'glibc', 'clang-cross-arm', 'compiler-rt', 'libcxx', 'ca-certificates-native', 'patch-native', 'pbzip2-native', 'gcc-runtime', 'zlib', 'util-linux', 'expat', 'freetype', 'libtool-native', 'xz-native', 'zlib-native', 'openssl-native', 'util-linux-libuuid-native', 'libffi-native', 'libnsl2-native', 'gdbm-native', 'readline-native', 'libtirpc-native', 'bzip2-native', 'ncurses-native', 'sqlite3-native', 'linux-libc-headers', 'clang-native', 'binutils-cross-arm', 'libgcc', 'attr-native', 'libcap-ng', 'ncurses', 'libpam', 'util-linux-libuuid', 'bash-completion', 'opkg-utils', 'libxcrypt', 'libpng', 'texinfo-dummy-native', 'gettext-minimal-native', 'perl-native', 'libedit-native', 'swig-native', 'cmake-native', 'binutils-native', 'libxml2-native', 'flex-native', 'gnu-config-native', 'cracklib', 'flex', 'libpcre-native', 'zstd-native', 'm4-native']
| DEBUG: Python function extend_recipe_sysroot finished
ERROR: Task (/home/gencay/STM32MPU_workspace/openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/meta-flutter/recipes-graphics/flutter-engine/flutter-engine_git.bb:do_install) failed with exit code '1'
Here is the complete error text:
2022-08-25 07:32 AM
Hi @Gencay
Did you try to contact @Community member owner of the layer ?
Also, did you take care that you are using Kirkstone while AFAIK the layer is only available/tested for dunfell ?
Olivier
2022-08-25 07:46 AM
@Gencay See the CI job for working reference: