cancel
Showing results for 
Search instead for 
Did you mean: 

How to make a SD-Card which is used to boot the system.

Jliu.21
Associate II

I have a question,I have no any USB-OTG interface can be used to help me burning and I can only use SD card to run my board. How can I make this SD-Card work only on linux command lines for example "dd" and so on. I have made tf-a uboot kernel(image) dtb and rootfs. I wish someone can help me ,thank you so much.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION
3 REPLIES 3
PatrickF
ST Employee

Hi @Jliu.2​ , Please click on 'Select as Best' if reply solved your issue or answered your question.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

thank you! already done!