Skip to main content
allard
Senior
January 27, 2021
Solved

Getting eMMC to boot

  • January 27, 2021
  • 1 reply
  • 1538 views

I’m having some trouble getting u-boot to boot from eMMC. I’ve evaluated my system using the DK2(using SDCARD) and i’m now porting to a custom board. The custom board contains a STM32MP157CAB and a eMCC connected at sdmmc2.

My u-boot devicetree(stm32mp157c-cau-mx-u-boot.dtsi) contains the following:

aliases {
		usb0 = &usbotg_hs;
		mmc0 = &sdmmc2;
	};

The first problem is the eMMC flashlayout file created by the distribution package, it is configured to use MMC1 by default. Is there a way to edit something that the file is created with MCC0 as default?

The second problem is with u-boot, it stills want to boot from MMC1:

NOTICE: CPU: STM32MP157CAB Rev.B
NOTICE: Model: <product name>
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: Using EMMC
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r1.0(debug):v2.2-dirty
NOTICE: BL2: Built : 13:36:23, Oct 22 2019
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffed000
INFO: Image id=4 loaded: 0x2ffed000 - 0x2ffff000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 848860
INFO: Image id=5 loaded: 0xc0100000 - 0xc01cf3dc
WARNING: Skip signature check (header option)
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffed000
INFO: SPSR = 0x1d3
INFO: Cannot find st,stpmic1 node in DT
NOTICE: SP_MIN: v2.2-r1.0(debug):v2.2-dirty
NOTICE: SP_MIN: Built : 13:36:23, Oct 22 2019
INFO: ARM GICv2 driver initialized
INFO: ETZPC: UART1 (3) could be non secure
INFO: ETZPC: SPI6 (4) could be non secure
INFO: ETZPC: I2C4 (5) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
 
 
U-Boot 2020.01-stm32mp-r1 (Jan 27 2021 - 09:28:31 +0000)
 
CPU: STM32MP157CAB Rev.B
Model: <product name>
Board: stm32mp1 in trusted mode (st,stm32mp157c-cau-mx)
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 200 MHz
- AXI : 266.500 MHz
- PER : 0 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment
 
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
Hit any key to stop autoboot: 0
Boot over mmc1!
Saving Environment to MMC... Writing to redundant MMC(0)... OK
MMC Device 1 not found
no mmc device at slot 1
STM32MP>

When I change the alias to mmc1 = &sdmcc2 u-boot stills throws the

MMC Device 1 not found
no mmc device at slot 1

error. The MMC is still reported with:

MMC: STM32 SD/MMC: 0

Also the orginal eMMC flashlayout file should work now, as I changed to MMC1, but it doesn’t, it causes the device to boot-loop.

What am I doing wrong?

I've found this topic, but i'm not sure if it is related.

This topic has been closed for replies.
Best answer by allard

Managed to fix this, for anyone coming across the same problem:

  1. Apply the fix in this topic, if still needed because ST will (?) fix this in the future.
  2. Edit the u-boot bootcmd using devtool(if distribution package). Usage of devtool can be found here.

The file to be edited is include/configs/stm32mp.h, change the define STM32MP_BOOTCMD to the following:

#define STM32MP_BOOTCMD "bootcmd_stm32mp=" \
	"echo \"Boot over ${boot_device}${boot_instance}!\";" \
	"if test ${boot_device} = serial || test ${boot_device} = usb;" \
	"then stm32prog ${boot_device} ${boot_instance}; " \
	"else " \
		"run env_check;" \
		"if test ${boot_device} = mmc;" \
		"then env set boot_targets mmc0; fi;" \
		"if test ${boot_device} = nand ||" \
		 " test ${boot_device} = spi-nand ;" \
		"then env set boot_targets ubifs0; fi;" \
		"if test ${boot_device} = nor;" \
		"then env set boot_targets mmc0; fi;" \
		"run distro_bootcmd;" \
	"fi;\0"

Not sure if this is the correct way to do this, but it works.

1 reply

allard
allardAuthorBest answer
Senior
January 29, 2021

Managed to fix this, for anyone coming across the same problem:

  1. Apply the fix in this topic, if still needed because ST will (?) fix this in the future.
  2. Edit the u-boot bootcmd using devtool(if distribution package). Usage of devtool can be found here.

The file to be edited is include/configs/stm32mp.h, change the define STM32MP_BOOTCMD to the following:

#define STM32MP_BOOTCMD "bootcmd_stm32mp=" \
	"echo \"Boot over ${boot_device}${boot_instance}!\";" \
	"if test ${boot_device} = serial || test ${boot_device} = usb;" \
	"then stm32prog ${boot_device} ${boot_instance}; " \
	"else " \
		"run env_check;" \
		"if test ${boot_device} = mmc;" \
		"then env set boot_targets mmc0; fi;" \
		"if test ${boot_device} = nand ||" \
		 " test ${boot_device} = spi-nand ;" \
		"then env set boot_targets ubifs0; fi;" \
		"if test ${boot_device} = nor;" \
		"then env set boot_targets mmc0; fi;" \
		"run distro_bootcmd;" \
	"fi;\0"

Not sure if this is the correct way to do this, but it works.