2019-10-04 02:59 AM
We need IBIS model file for STM32MP157AAD3 Processor. Please send or share the link to download.
2019-10-04 04:08 AM
Hello,
IBIS models are available on STM32MP157A resources page : https://www.st.com/resource/en/bsdl_model/stm32mp1_ibis.zip
2019-10-04 06:11 AM
Hi,
We have done the schematic design using STM32MP157AAD3 Processor. We need to know the design review from your side so please let me know can you review the schematic.
We are using PMIC STPMIC1APQR, LDO5OUT is 1.7v to 3.9v by default 3.3v , We have to generate 3.7V so How it can be done?
Thanks & Regards
Priya S
2019-10-07 01:24 AM
Hi @PS.5
Please refer to STPMIC1 Datasheet
https://www.st.com/resource/en/datasheet/stpmic1.pdf
LDO5OUT is 2.9V, enable RANK2 by default.
For generating 3.7V, you need to disable the automatic start by setting it RANK0 in NVM.
Then set it @3.7V and enable it at runtime.
Hope it help,
Olivier
2019-10-07 01:40 AM
Hello,
We did not do schematic review.
In some cases, if you are served in direct by ST, is it possible to ask for some sanity check.
Only in that case, you could ask for support to your ST local FAE.
Regards.