2024-09-30 2:42 AM
Hello forum;
I needed help to do some SI simulation on ESDALC6V1-5M6 and LD39150PU33R Hyperlynx/Altium Designer SI simulator. Hence my question is does this ibis model exist? If yes where can I download it?
2024-10-01 6:30 AM
Hi,
I fear IBIS are not available for ESD protection devices. Maybe a simple hand-made model could be used (using the information in product datasheet).
For LDOs, I wonder what could be the link with high-speed signal integrity simulation. I guess IBIS model does not apply at all power devices like LDOs.
Regards.
2024-10-01 6:50 AM
You can use Altium designer. You can manually add parasitic parameters (like capacitance, resistance, and inductance) for ESD components.