2023-03-16 5:15 PM
Hi,
I try to connect ADC channels with libiio for my custom board based on the stm32mp157caa3. I followed the instructions from the link
https://wiki.st.com/stm32mpu/wiki/IIO_libiio
https://wiki.st.com/stm32mpu/wiki/ADC_device_tree_configuration#DT_configuration_examples
but without success. After issuing the console
iio_info
I get
Library version: 0.23 (git tag: 92d6a35)
Compiled with backends: local xml ip usb serial
IIO context created with local backend.
Backend version: 0.23 (git tag: 92d6a35)
Backend description string: Linux stm32mp1-connect-bridge 5.15.67 #1 SMP PREEMPT Thu Sep 8 10:32:54 UTC 2022 armv7l
IIO context has 2 attributes:
local,kernel: 5.15.67
uri: local:
IIO context has 0 devices:
The same is in
/sys/bus/iio/devices/
empty, with no devices.
Part of my dts looks
&adc{
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
status = "okay";
/* USER CODE BEGIN adc */
vdda-supply = <&vdda>; /* Example to supply vdda pin by using a PMIC regulator */
vref-supply = <&vrefbuf>; /* Example to use VREFBUF (It needs to be enabled as well) */
adc1: adc@0 {
assigned-resolution-bits = <12>;
/* Single-ended channels */
channel@0 {
reg = <0>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@2 {
reg = <2>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@12 {
reg = <12>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
channel@17 {
reg = <17>;
st,min-sample-time-ns = <10000>; /* 10µs sampling time */
};
};
/* USER CODE END adc */
};
In the Kernel configuration, I also marked
Device Drivers --->
<*> Industrial I/O support --->
Analog to digital converters --->
<*> STMicroelectronics STM32 adc core
<*> STMicroelectronics STM32 adc
It must be something I missed.
Thanks in advance for the hints.
BR Michal
Solved! Go to Solution.
2023-05-08 10:09 AM
After some break and rechecking everything I discover a correct dts configuration.
First I used as reference AVDD(external) and according to this I have configurations like
The Kernel
&adc {
/* ANA0, ANA1 are dedicated pins and don't need pinctrl: only in6. */
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
vdd-supply = <&vdd>;
vdda-supply = <&vdda>;
vref-supply = <&vdda>;
status = "okay";
adc1: adc@0 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
channel@0 {
reg = <0>;
/* 16.5 ck_cycles sampling time */
st,min-sample-time-ns = <5000>;
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <5000>;
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <5000>;
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <5000>;
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <5000>;
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <5000>;
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <5000>;
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <5000>;
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <5000>;
};
};
};
The U-Boot
&adc {
/* ANA0, ANA1 are dedicated pins and don't need pinctrl: only in6. */
pinctrl-names = "default", "sleep";
pinctrl-0 = <&adc_pins_mx>;
pinctrl-1 = <&adc_sleep_pins_mx>;
vdd-supply = <&vdd>;
vdda-supply = <&vdda>;
vref-supply = <&vdda>;
status = "okay";
adc1: adc@0 {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
channel@0 {
reg = <0>;
/* 16.5 ck_cycles sampling time */
st,min-sample-time-ns = <5000>;
};
channel@1 {
reg = <1>;
st,min-sample-time-ns = <5000>;
};
channel@3 {
reg = <3>;
st,min-sample-time-ns = <5000>;
};
channel@5 {
reg = <5>;
st,min-sample-time-ns = <5000>;
};
channel@6 {
reg = <6>;
st,min-sample-time-ns = <5000>;
};
channel@9 {
reg = <9>;
st,min-sample-time-ns = <5000>;
};
channel@10 {
reg = <10>;
st,min-sample-time-ns = <5000>;
};
channel@13 {
reg = <13>;
st,min-sample-time-ns = <5000>;
};
channel@15 {
reg = <15>;
st,min-sample-time-ns = <5000>;
};
};
};
Finally T-Fa
&etzpc{
status = "okay";
st,decprot = <
/*"Non Secured" peripherals*/
DECPROT(STM32MP1_ETZPC_ADC_ID, DECPROT_NS_RW, DECPROT_UNLOCK)
...
}
and
&rcc{
...
CLK_ADC_PLL4R
pll4:st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 3 98 5 6 5 PQR(1,1,1) >;
};
This works for me and maybe will be suitable for someone else.
Thanks for any help
Topic can be closed.
2023-03-17 2:57 AM
Hi MWoło.2 (Community Member)
According to https://www.kernel.org/doc/Documentation/devicetree/bindings/iio/iio-bindings.txt
It seems that you may have missed the #io-channel-cells = <1>; property in the ADC node.
from : linux-5.15.67/arch/arm/boot/dts/stm32mp151.dtsi
adc: adc@48003000 {
compatible = "st,stm32mp1-adc-core";
reg = <0x48003000 0x400>;
...
adc1: adc@0 {
compatible = "st,stm32mp1-adc";
#io-channel-cells = <1>;
...
Regards,
Olivier
2023-03-17 6:47 AM
Hi OlivierK,
thanks for the hint, unfortunately, it doesn't work. It is curious to that my configuration works for the DK2 board, in DK2 I see iio devices. The difference between my custom and dk2 is that dk2 not uses cube mx.
2023-03-17 6:48 AM
In my opinion, the system doesn't bind adc driver with iio. How to force the system to bind adc with iio?
2023-03-17 7:49 AM
Hi MWoło.2 (Community Member)
Regarding the bindings, you can use CubeMx and generate MP15-DK2 dts and compare with your settings. Normally if the IIO is enabled in the kernel I don't see why it shouldn't work.
2023-03-17 8:08 AM
OK,
let's compare
after issue
grep -H "" /sys/bus/iio/devices/*/name | grep adc
I get on my board
grep: /sys/bus/iio/devices/*/name: No such file or directory
and on disco
/sys/bus/iio/devices/iio:device0/name:48003000.adc:adc@0
What do the above means? If I get "No such file ...." it means not configured something in the kernel config or missing something in dts?
2023-03-17 8:10 AM
The configuration of both board
I can't find only the U-Boot drivers
Do U-Boot configuration (dts+driver) significant?
2023-03-17 8:17 AM
Hi MWoło.2 (Community Member)
What about the diff between CubeMX DTS generation for the MP15-DK2 vs your board?
2023-03-17 8:32 AM
Hi,
you can try something like this
&adc1 {
st,min-sample-time-nsecs = <10000000>;
st,adc-channels = <9 19>;
assigned-resolution-bits = <12>;
status = "okay";
};
This works for me on STe4.1.
2023-03-17 8:49 AM
ok I try, thanks