cancel
Showing results for 
Search instead for 
Did you mean: 

After upgrade to 4.1 (Kirkstone) tf-a boot failure

GLaure
Senior

Hi,

I upgraded the image for our custom board to 4.1 last week. After fixing the sw issues

concerning the recipe syntax changes i have now problems to boot the new image.

Info: Our board does not use PMIC but static voltage configuration:

/ {
	model = "DEWETRON NEXDAQ tf-a";
	compatible = "st,stm32mp157f-nexio", "st,stm32mp157";
 
	aliases {
		serial0 = &uart4;
		serial1 = &usart1;
		serial2 = &usart2;
	};
 
	chosen {
		stdout-path = "serial0:115200n8";
	};
 
	/* Supply Voltages */
	vddcore: vddcore {
		regulator-name = "vddcore";
		regulator-min-microvolt = <1200000>;
		regulator-max-microvolt = <1350000>;
		regulator-always-on;
	};
 
	vdd: vdd {
		regulator-name = "vdd";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-always-on;
	};
 
	v3v3: v3v3 {
		regulator-name = "v3v3";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-always-on;
	};
 
	vdd_usb: vdd_usb {
		regulator-name = "vdd_usb";
		regulator-min-microvolt = <3300000>;
		regulator-max-microvolt = <3300000>;
		regulator-always-on;
	};
 
};

With this coniguration the boot fails with these messages:

NOTICE:  CPU: STM32MP157FAC Rev.Z
NOTICE:  Model: DEWETRON NEXDAQ tf-a
WARNING: regulator_get_by_phandle: phandle 10 not found
WARNING: VDD unknown
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO:    FCONF: Reading firmware configuration information for: stm32mp_io
INFO:    Using SDMMC
INFO:      Instance 1
INFO:    Boot used partition fsbl1
WARNING: regulator_get_by_phandle: phandle 14 not found
NOTICE:  BL2: v2.6-stm32mp1-r2.0(debug):v2.6-dirty(a1f02f4f)
NOTICE:  BL2: Built : 13:14:26, Nov 23 2021
ERROR:   Unable to find a metadata partition
WARNING: Failed to set reference to image id=12 (-2)
WARNING: loading of FWU-Metadata failed, using Bkup-FWU-Metadata
ERROR:   Unable to find a metadata partition
WARNING: Failed to set reference to image id=13 (-2)
ERROR:   loading of Bkup-FWU-Metadata failed
PANIC at PC : 0x2ffea21b

With 3.1 and tf-a 2.6 the boot log was this:

NOTICE:  CPU: STM32MP157FAC Rev.Z
NOTICE:  Model: DEWETRON NEXDAQ tf-a
WARNING: regulator_get_by_phandle: phandle 17 not found
WARNING: VDD unknown
INFO:    Reset reason (0x15):
INFO:      Power-on Reset (rst_por)
INFO:    FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO:    FCONF: Reading firmware configuration information for: stm32mp_io
INFO:    Using EMMC
INFO:      Instance 2
INFO:    Boot used partition fsbl1
WARNING: regulator_get_by_phandle: phandle 21 not found
NOTICE:  BL2: v2.4-r2.0(debug):v2.4-dirty
NOTICE:  BL2: Built : 16:43:51, Nov 17 2020
INFO:    BL2: Doing platform setup
INFO:    RAM: DDR3-DDR3L 16bits 533000kHz
INFO:    Memory size = 0x20000000 (512 MB)
INFO:    BL2: Loading image id 31
INFO:    Loading image id=31 at address 0x2ffff000
INFO:    Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO:    FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO:    FCONF: Reading firmware configuration information for: dyn_cfg
INFO:    FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO:    BL2: Loading image id 4
INFO:    Loading image id=4 at address 0x2ffc5000
INFO:    Image id=4 loaded: 0x2ffc5000 - 0x2ffd97ec
WARNING: Not a known TEE, use default loading options.
INFO:    BL2: Skip loading image id 21
INFO:    BL2: Skip loading image id 22
INFO:    BL2: Loading image id 23
INFO:    Loading image id=23 at address 0xc0500000
INFO:    Image id=23 loaded: 0xc0500000 - 0xc051cbba
INFO:    BL2: Loading image id 26
INFO:    Loading image id=26 at address 0x2ffc0000
INFO:    Image id=26 loaded: 0x2ffc0000 - 0x2ffc3cb9
INFO:    BL2: Loading image id 5
INFO:    Loading image id=5 at address 0xc0100000
INFO:    Image id=5 loaded: 0xc0100000 - 0xc01d3ee8
NOTICE:  BL2: Booting BL32
INFO:    Entry point address = 0x2ffc5000
INFO:    SPSR = 0x1d3
NOTICE:  SP_MIN: v2.4-r2.0(debug):v2.4-dirty
NOTICE:  SP_MIN: Built : 16:43:51, Nov 17 2020
INFO:    ARM GICv2 driver initialized
INFO:    Set calibration timer to 44 sec
INFO:    stm32mp1 IWDG1 is secure
INFO:    SP_MIN: Initializing runtime services
INFO:    SP_MIN: Preparing exit to normal world
 
 
U-Boot 2020.10-stm32mp-r2 (Oct 05 2020 - 15:15:32 +0000)

​(Yes this is eMMC but thats selected by the dip switches)

Does anyone has an idea what I can do?

Currently studying:

https://community.st.com/s/article/FAQ-STM32MP1-bring-up-troubleshooting-guide

Bye Gunther

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
GLaure
Senior
2 REPLIES 2
GLaure
Senior

Found:

https://community.st.com/s/question/0D53W00001lRWkjSAG/stm32mp157fdk2-failing-to-boot-on-custom-image

As I am using a custom tsv file, no tool mentioned a missing metadata.bin.

GLaure
Senior

The missing metadata.bin was the issue.