2023-01-17 01:33 AM
2023-01-17 08:00 AM
Hi @eeng.1
unfortunately, there is very few details on your module, if SPI or similar interface, might probably need SW driver customization where we cannot help much.
With STM32MP157x-DK1/DK2 boards, to add a 2nd Ethernet port, it would be more straightforward to use such USB Type-A<->Ethernet module which is widely available and should work with default Starter Package.
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-01-17 08:00 AM
Hi @eeng.1
unfortunately, there is very few details on your module, if SPI or similar interface, might probably need SW driver customization where we cannot help much.
With STM32MP157x-DK1/DK2 boards, to add a 2nd Ethernet port, it would be more straightforward to use such USB Type-A<->Ethernet module which is widely available and should work with default Starter Package.
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2023-02-16 06:43 AM
I bought a USB type A to ethernet converter and it worked perfectly. (with speed 100Mbps). Thanks a lot.