2021-10-14 8:18 AM
root@stm32mp1:~# timedatectl status
Local time: Thu 2021-10-14 15:10:06 UTC
Universal time: Thu 2021-10-14 15:10:06 UTC
RTC time: Sat 2000-01-01 00:00:38
Time zone: UTC (UTC, +0000)
System clock synchronized: no
NTP service: active
RTC in local TZ: no
My RTC is out of sync.
This is the date loaded after every boot. Where does system clock get it?
This is the timesyncd service.
[[0;1;32m*[[0m systemd-timesyncd.service - Network Time Synchronization
Loaded: loaded (/lib/systemd/system/systemd-timesyncd.service; enabled; vendor preset: enabled)
Active: [[0;1;32mactive (running)[[0m since Thu 2021-10-14 15:09:43 UTC; 2min 23s ago
Docs: man:systemd-timesyncd.service(8)
Main PID: 373 (systemd-timesyn)
Status: "Idle."
Memory: 576.0K
CGroup: /system.slice/systemd-timesyncd.service
`-373 /lib/systemd/systemd-timesyncd
Sep 20 10:44:02 stm32mp1 systemd[1]: Starting Network Time Synchronization...
Sep 20 10:44:03 stm32mp1 systemd-timesyncd[373]: System clock time unset or jumped backwards, restoring from recorded timesta
mp: Thu 2021-10-14 15:09:43 UTC
Oct 14 15:09:43 stm32mp1 systemd[1]: Started Network Time Synchronization.
I already tried:
hwclock -w, then rebooting, then hwclock -s, but it goes back to 2000s.
Can someone help me?
Solved! Go to Solution.
2021-10-15 12:59 AM
Ok, I got the point.
You wanted to save the current system time as the 'last ntp time' which is the one restored at boot time. right ?
I'm not SW expert, but I found that which seems working. Don't know if it is a reliable solution.
date -s "fri oct 15 09:54:00 UTC 2021" <-- if needed
touch /var/lib/systemd/timesync/clock
sync
I hope other people from community have some more clever answers.
Regards.
2021-10-14 9:19 AM
Hi,
to 'copy' system time to RTC, you need to use the following:
hwclock --systohc --utc
See https://wiki.st.com/stm32mpu/wiki/How_to_use_the_RTC
Obviously, need a 3V battery on VBAT pin to keep time in absence of power.
Regards.
2021-10-15 12:15 AM
The point is my cmos battery is dead, but somehow at boot, time is not the RTC reset time (Sat 2000-01-01 00:00:38), but is restored to the last time that there was an internet connection (i think it's the ntp service that does this). However this time does not keep the progress while the board is running offline. How can i update this time, so that it accounts for the time the board is on but offline at the next reboot?
Thanks
2021-10-15 12:59 AM
Ok, I got the point.
You wanted to save the current system time as the 'last ntp time' which is the one restored at boot time. right ?
I'm not SW expert, but I found that which seems working. Don't know if it is a reliable solution.
date -s "fri oct 15 09:54:00 UTC 2021" <-- if needed
touch /var/lib/systemd/timesync/clock
sync
I hope other people from community have some more clever answers.
Regards.
2021-10-15 2:17 AM
Thanks for your help, but stil can't achieve what i want.
As you suggest, the documentation says:
"/var/lib/systemd/timesync/clock
The modification time ("mtime") of this file is updated on each successful NTP synchronization or after each
SaveIntervalSec= time interval, as specified in timesyncd.conf(5). At the minimum, it will be set to the systemd build date. It is used to ensure that the system clock remains roughly monotonic across reboots, in case no local RTC is available."
When i connect to internet and ntp gets a new date, the modification time of the file changes, but if i try to add SaveIntervalSec inside timesyncd.conf i get that the service does not know the variable
Oct 15 08:52:01 stm32mp1 systemd-timesyncd[1171]: [[0;1;38;5;185m[[0;1;39m[[0;1;38;5;185m/etc/systemd/timesyncd.conf:6: Unkno
wn key name 'SaveIntervalSec' in section 'Time', ignoring.[[0m
I think i'll just call a script that does "touch /var/lib/systemd/timesync/clock" periodically.
Thanks again for the help
Have a nice day
2021-10-15 2:44 AM
Hi,
Seems the 'SaveIntervalSec' is not supported in the Linux we use (don't ask me why, I'm an HW guy !).
Regards,
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'