cancel
Showing results for 
Search instead for 
Did you mean: 

Can't connect to STM32

huan123
Associate

I'm encountering difficulties while attempting to connect and debug my STM32 microcontroller, and I'm seeking guidance from the community. I have erased the full chip flash memory and uploaded my code but suddenly I start getting these error messages,

Error Messages:
1. In ST-Link Utility:

Can not connect to target!
If you're trying to connect to an STM32W1xx device, please select Normal or HotPlug mode from Target->Settings menu.
If you're trying to connect to a low-frequency application, please select a lower SWD Frequency mode from Target->Settings menu.

1 REPLY 1

Welcome to the community.

Please see the posting tips:

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

I've edited your post title as, "Hello ST Community" doesn't identify what your post is about.

 


@huan123 wrote:

I'm encountering difficulties while attempting to connect and debug my STM32 microcontroller, .


You say microcontroller (aka "MCU"), but you've posted in the MPU section.

What chip are you using? The thread can be moved if required.

Also please give board details.

 


@huan123 wrote:

In ST-Link Utility:


Note that the old ST-Link Utility has been replaced for many years by the STM32CubeProgrammer:

https://www.st.com/en/development-tools/stm32cubeprog.html

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.