cancel
Showing results for 
Search instead for 
Did you mean: 

Exit Low Power Mode M4 via CAN

YRink.1
Associate II

Hi,

i have a question regarding to exit the Low Power Mode on CM4. Is it possible that i can exit the CStop or CStandby Mode via an Rx Messages of the CAN Bus, when the CAN Bus is assigned to the M4. Iam confused because almost every Bus is listed in https://wiki.st.com/stm32mpu/wiki/Coprocessor_power_management as Wake Up Source except the CAN Bus.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

I confirm, the HW does not permit that.

See STM32MP15x Reference Manual, PWR section.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.