Skip to main content
JWeis.3
Associate
January 13, 2021
Solved

Is it possible to run the qt5 3d demos with a openstlinux-eglfs build (STM32MP157C-DK2)?

  • January 13, 2021
  • 2 replies
  • 1670 views

I created an eglfs Yocto build that can run the simple Qt5 demos, but I'm seeing fairly high CPU usage and I'm trying to figure out if the GPU is being used. I pondered that the GPU may not accelerate 2D graphics very well and does better with actual 3D. So, I thought I'd add support for more Qt5 packages and see if the 3d demos ran any better, but I can't get it to build.

I'm getting a compiler error while building QT5's ogl-runtime complaining that <GLES2.gl3.h> cannot be found. I'm new to this, but from what I can tell this header should be supplied with the opengl libraries and presumably ST should be supplying that library with GPU acceleration.

Or perhaps something else is going wrong/missing?

Is it possible to get the Qt5 3D demos to run under an eglfs build? Is there some way to verify if the GPU is being used?

Thanks,

Jon

======

In file included from /home/jon/STM32MP15/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/ogl-runtime/2.5.0+gitAUTOINC+25236c672d_31697c758f-r0/git/src/engine/EnginePrefix.h:33,

         from /home/jon/STM32MP15/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/ogl-runtime/2.5.0+gitAUTOINC+25236c672d_31697c758f-r0/git/src/engine/Qt3DSRenderRuntimeBindingImplRenderer.cpp:30:

/home/jon/STM32MP15/Distribution-Package/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/ogl-runtime/2.5.0+gitAUTOINC+25236c672d_31697c758f-r0/git/src/render/backends/gl/Qt3DSOpenGLPrefix.h:40:10: fatal error: GLES3/gl3.h: No such file or directory

  40 | #include <GLES3/gl3.h>

   |     ^~~~~~~~~~~~~

compilation terminated.

=================

Build Configuration:

BB_VERSION      = "1.46.0"

BUILD_SYS      = "x86_64-linux"

NATIVELSBSTRING   = "universal"

TARGET_SYS      = "arm-ostl-linux-gnueabi"

MACHINE       = "stm32mp1"

DISTRO        = "openstlinux-eglfs"

DISTRO_VERSION    = "3.1-snapshot-20210113"

TUNE_FEATURES    = "arm vfp cortexa7 neon vfpv4 thumb callconvention-hard"

TARGET_FPU      = "hard"

DISTRO_CODENAME   = "dunfell"

ACCEPT_EULA_stm32mp1 = "1"

GCCVERSION      = "9.%"

PREFERRED_PROVIDER_virtual/kernel = "linux-stm32mp"

meta-python      

meta-oe        

meta-gnome      

meta-xfce       

meta-initramfs    

meta-multimedia    

meta-networking    

meta-webserver    

meta-filesystems   

meta-perl      = "HEAD:b5f510e48080b6dc710ff4800feb90ef679c5456"

meta-st-stm32mp   = "HEAD:7a1ab80ccb655e9cd28c9ea8a4a83fca48c48b11"

meta-qt5       = "HEAD:ac7514e2bc295c97faa86d24e8823829257adbb8"

meta-st-openstlinux = "HEAD:5465ed3781355776cb46d2cc45884b1ccc1011cd"

meta         = "HEAD:1795f30d8ab73d35710ca99064c51190dc84853e"

This topic has been closed for replies.
Best answer by AntonioST

@JWeis.3​ I would suggest you to check in the wiki page How to build and use an SDK for QT for your case.

The include file <GLES3/gl3.h> is not present because openGLES 3 is not supported. I suspect there is an incorrect configuration in your build.

To measure the GPU loading you can use the script in the wiki page How to monitor the GCNANO GPU load.

2 replies

AntonioST
AntonioSTBest answer
ST Employee
January 18, 2021

@JWeis.3​ I would suggest you to check in the wiki page How to build and use an SDK for QT for your case.

The include file <GLES3/gl3.h> is not present because openGLES 3 is not supported. I suspect there is an incorrect configuration in your build.

To measure the GPU loading you can use the script in the wiki page How to monitor the GCNANO GPU load.

JWeis.3
JWeis.3Author
Associate
January 19, 2021

Thank you Antonio. It looks like my build (before I tried adding support for Q5t's 3D objects) was using the GPU.

We'll need to see next if there's a way to improve the performance of Qt5's graphics as even with the GPU clearly helping out, the CPU usage is still quite high for simple graphical animations.