cancel
Showing results for 
Search instead for 
Did you mean: 

Device don't load u-boot after uploaded with STM32_Programmer_CLI

Adrian1
Associate III

I changed name of orginal device-tree of my board stm32mp157c-dk2.dts. Then I tried upload tf-a and uboot to device via STM32_Programmer_CLI. Program proper uploaded tf-a and I see my new Model name but now program wait for reconnecting and my device is hald.

WARNING: Skip signature check (header option)
NOTICE:  ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE:  BL2: Booting BL32
INFO:    Entry point address = 0x2ffed000
INFO:    SPSR = 0x1d3
NOTICE:  SP_MIN: v2.2-r1.0(debug):v2.2-dirty
NOTICE:  SP_MIN: Built : 13:36:23, Oct 22 2019
INFO:    ARM GICv2 driver initialized
INFO:    stm32mp IWDG1 (12): Secure
INFO:    SP_MIN: Initializing runtime services
INFO:    SP_MIN: Preparing exit to normal world

I don't get any error so I don't know what can be wrong. When I uploaded the same device-tree but with original name u-boot is booting

regards,

Adrian

5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @Adrian Dusiński​ 

Not clear what you have done exactly.

Did you recompile Tf-a and Uboot using a renamed/custom dts file ?

Could you please details steps you follow ?

Please precise if you are working with ecosystem V1.x ( kernel 4.19) or V2.0 ( kernel 5.4 )

Thanks

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi,

Thanks for response.

To be exact I try this:

https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board

I copied original stm32mp157c-dk2 device-tree to stm32mp157-custom, I added this configuration to makefile and I executed:

make stm32mp15_trusted_defconfig

make DEVICE_TREE=stm32mp157c-custom all

So my configuration is the same as stm32mp157c-dk2.

I also tried set debug to tf-a but it end program after console_flush(); so it works. I don't know how get more debug.

Regards,

Adrian

Adrian1
Associate III

I found the problem, in the "board/st/stm32mp1/extlinux.conf" file must be added custom devicetree.

I think on the page "How to configure U-Boot for your board" is no information about it.

Regards,

Adrian

Hi Adrian

I also met this problem. How can I solve it.

Regards,

User.44

PDELA.1
Associate II

Hi Adrian,

I don't understood extlinux.conf refence here....

it is not used for STM32CubeProgrammer load.

To start your custom device tree for U-Boot based on DK2 :

cp arch/arm/dts/stm32mp157c-dk2.dts arch/arm/dts/stm32mp157-custom.dts

it is the kernel device tree

cp arch/arm/dts/stm32mp157c-dk2-u-boot.dtsi arch/arm/dts/stm32mp157-custom-u-boot.dtsi

this add-on U-Boot file (stm32mp157-custom-u-boot.dtsi) is MANDATORY to manage u-boot specific property needed in pre-reloc step:

attribute u-boot,dm-pre-reloc / u-boot,dm-pre-proper => https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#Device_tree.

Update arch/arm/dts/Makefile to compile your device tree:

dtb-$(CONFIG_STM32MP15x) +=stm32mp157-custom.dtb

Then launch compilation

make DEVICE_TREE=stm32mp157c-custom all

Patrick