2022-02-10 9:07 PM
Hello,
I have sd card with lots of things configured.To save time I want to create backup of this card which I can flash later.
Is there any official way to take the backup of the STM32MPU sd card image and also a way to flash the same image on new SD card (with the starter package already installed as well as a new card from the factory ).
Looking for an STM32MPU DK2 F board but I think must be valid for all boards
Regards,
Thanks in Advance !
2022-02-10 11:49 PM
Hi @darla14 ,
See this community post already addressing same question :
Olivier
2022-02-10 11:51 PM
Found also this one https://community.st.com/s/question/0D53W00000BqJHLSA3/save-linux-image