cancel
Showing results for 
Search instead for 
Did you mean: 

Creating a flashable backup of sd card image

darla14
Senior

Hello,

I have sd card with lots of things configured.To save time I want to create backup of this card which I can flash later.

Is there any official way to take the backup of the STM32MPU sd card image and also a way to flash the same image on new SD card (with the starter package already installed as well as a new card from the factory ).

Looking for an STM32MPU DK2 F board but I think must be valid for all boards

Regards,

Thanks in Advance !

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @darla14​ ,

See this community post already addressing same question :

https://community.st.com/s/question/0D53W00000qwKLQSA2/how-to-backup-partitions-from-sd-card-image-and-to-flash-it-later

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Found also this one https://community.st.com/s/question/0D53W00000BqJHLSA3/save-linux-image

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.