Change default tf-a and u-boot serial linux console.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-25 6:29 AM
Hello, my main seriale console should be USART2 instead of UART4. I modified the kernel dts as follows:
chosen {
stdout-path = "serial0:115200n8";
};
aliases {
ethernet0 = ðernet0;
mmc0 = &sdmmc1;
mmc1 = &sdmmc2;
serial0 = &usart2;
};
and it configures correctly the kernel console.
If I try the same modification in tf-a and u-boot dts, at boot i see the log starting on uart4, but it blocks at this point
Preparing exit to normal world
No serial driver found
Should I modify some boot env too?
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-28 2:05 AM
Hi, I have this log on uart4 (even if it should be disabled)
NOTICE: CPU: STM32MP157CAA Rev.Z
NOTICE: Model: STMicroelectronics STM32MP157C eval daughter on eval mother
INFO: Reset reason (0x14):
INFO: Pad Reset from NRST
INFO: PMIC version = 0x21
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe3000
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.4-r1.0(debug):4d81224-dirty
NOTICE: BL2: Built : 13:23:30, Jun 15 2021
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 32bits 533000Khz
WARNING: Couldn't find property st,phy-cal in dtb
INFO: Memory size = 0x40000000 (1024 MB)
INFO: DFU USB START...
INFO: phase ID :0, Manifestation 0 at c0000244
INFO: phase ID :3, Manifestation 3 at c8101006
INFO: Send detach request
INFO: Receive DFU Detach
INFO: DFU USB STOP...
INFO: BL2: Loading image id 31
INFO: Loading image id=31 at address 0x2ffff000
INFO: Image id=31 loaded: 0x2ffff000 - 0x2ffff226
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc5000
INFO: Image id=4 loaded: 0x2ffc5000 - 0x2ffd847c
WARNING: Not a known TEE, use default loading options.
INFO: BL2: Skip loading image id 21
INFO: BL2: Skip loading image id 22
INFO: BL2: Loading image id 23
INFO: Loading image id=23 at address 0xc0500000
INFO: Image id=23 loaded: 0xc0500000 - 0xc051e86c
INFO: BL2: Loading image id 26
INFO: Loading image id=26 at address 0x2ffc0000
INFO: Image id=26 loaded: 0x2ffc0000 - 0x2ffc47f8
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc01ca800
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc5000
INFO: SPSR = 0x1d3
this is the log of the programmer cli:
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 003400463030510139393639
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: debug-tf-a-stm32mp157c-ev1-usb.stm32
File : debug-tf-a-stm32mp157c-ev1-usb.stm32
Size : 225656 Bytes
Partition ID : 0x01
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:00.486
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
██████████████████████████████████████████████████ 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: stm32mp157c_eutron_mtb_fip.bin
File : stm32mp157c_eutron_mtb_fip.bin
Size : 1052678 Bytes
Partition ID : 0x03
Download in Progress:
██████████████████████████████████████████████████ 100%
File download complete
Time elapsed during download operation: 00:00:01.395
RUNNING Program ...
PartID: :0x03
Reconnecting the device ...
Error:
Unable to reconnect the target device: time out expired
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-10-28 6:09 AM
Hello,
Can I have your .tsv file please?
And did you replace the tf-a used inside your tsv, by the new one generated with the developer package?
Because the name of the tf-a downloaded: debug-tf-a-stm32mp157c-ev1-usb.stm32 looks like the default binary delivered by the starter package.
Just a reminder to how to use the tsv file: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#Updating_partitions
Did you have some traces on USART2, too?
Regards,
Kevin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-10 1:22 AM
Hello @Lmoio.1 ,
Did you fix your problem with CubeProgrammer?
Regards,
Kevin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-10 3:30 AM
Usually I generate a new fip binary and update that one in the .tsv, I leave stm32 as default.
Anyway, now it seems to work with the new uart after adding new address in CONFIG_DEBUG_UART_BASE.
Thank you
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-12 4:04 AM
Hello,
I have the same issue in my new board with STM32MP151aaaa SoC.
We decided to use the USART1 as DEBUG console, so the device-tree generated by STMCubeMX (with slightly adaption [i.e. some includes and a specific chosen=... node and u-boot,dm-pre-reloc]) and write over an SD Card to boot up from it.
Enabling the USART1 in the SPL mode:
#ifdef CONFIG_DEBUG_UART_BOARD_INIT
void board_debug_uart_init(void)
{
#if (CONFIG_DEBUG_UART_BASE == STM32_USART1_BASE)
/* On EUREK EK440 Board we are using USART1_TX and USART1_RX with PINS
* Uart1 TX = Z7
* Uart1 RX = Z6
*/
#define RCC_MP_APB5ENSETR (STM32_RCC_BASE + 0x0208)
#define RCC_MP_AHB5ENSETR (STM32_RCC_BASE + 0x0210)
/* UART1 clock enable */
setbits_le32(RCC_MP_APB5ENSETR, BIT(4));
#define GPIOZ_BASE 0x54004000
/* GPIOZ clock enable */
writel(BIT(0), RCC_MP_AHB5ENSETR);
/* GPIO configuration for EUREK EK440 boards: Uart1 TX = Z7, RX = Z6 */
/* GPIOx_MODER Z6 and Z7 = 31..0
* 1111 1111 1111 1111
* 1010 1111 1111 1111 --> MODER7 & MODER6 (Z7 and Z6)
*/
writel(0xffffafff, GPIOZ_BASE + 0x00);
/* GPIOZ GPIOx_AFRL AFR7 for PIN 7 & PIN 6
* 0111 0111 0000 0000 ---> AFR7 and AFR6
* 0000 0000 0000 0000
*/
writel(0x77000000, GPIOZ_BASE + 0x20);
#else
#error("CONFIG_DEBUG_UART_BASE: not supported value")
#endif
}
#endif
and adding the correct setup in .dts file as:
aliases {
u-boot,dm-pre-reloc;
ethernet0 = ðernet0;
serial0 = &XX_DEBUG_UART_XX;
serial1 = &usart2;
serial2 = &XX_NORMAL_UART_XX;
serial3 = &uart4;
};
chosen {
u-boot,dm-pre-reloc;
stdout-path = "serial0:115200n8";
};
Where XX_DEBUG_UART_XX is usart1 and XX_NORMAL_UART_XX is usart3
On serial debug (i.e. over a usart1 adapter over an FTDI 232RL Chip) I am able to see the SPL running on boot as I can see:
pinctrl_stm32 pin-controller@50002000: periph->name = serial@5c000000
serial_stm32 serial@5c000000: prop pinctrl-0 index 0 invalid phandle
clk id 148 not found
serial_stm32 serial@5c000000: failed to enable clock
And after that, I can see the following (I suppose it is u-boot SSBL or something different from above, because last two lines)
pinctrl_stm32 pin-controller@50002000: periph->name = serial@5c000000
serial_stm32 serial@5c000000: prop pinctrl-0 index 0 invalid phandle
clk id 148 not found
serial_stm32 serial@5c000000: failed to enable clock
No serial driver found
resetting ...
And it loops forever.
I have already checked the rcc node is under the u-boot,dm-pre-reloc because I am suspecting the phandle of pinctrl-0 clk 148 is not in the device-tree node somewhere...
Can you explain that?
Regards,
Gianluca
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-12 4:52 AM
Hi,
For the uboot project , I added CONFIG_DEBUG_UART_BASE=0x4000E000 (usart2 base address) in the defconfig, I added
chosen {
stdout-path = "serial0:115200n8";
};
aliases {
ethernet0 = ðernet0;
mmc0 = &sdmmc1;
mmc1 = &sdmmc2;
serial0 = &usart2;
serial1 = &uart4;
};
&pinctrl {
usart2_pins_d: usart2-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, AF7)>; /* USART2_TX */
bias-disable;
drive-push-pull;
slew-rate = <3>;
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
bias-pull-up;
};
};
usart2_idle_pins_d: usart2-idle-2 {
pins1 {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>; /* USART2_TX */
};
pins2 {
pinmux = <STM32_PINMUX('D', 6, AF7)>; /* USART2_RX */
bias-disable;
};
};
usart2_sleep_pins_d: usart2-sleep-2 {
pins {
pinmux = <STM32_PINMUX('D', 5, ANALOG)>, /* USART2_TX */
<STM32_PINMUX('D', 6, ANALOG)>; /* USART2_RX */
};
};
};
&usart2 {
pinctrl-names = "default", "sleep", "idle";
pinctrl-0 = <&usart2_pins_d>;
pinctrl-1 = <&usart2_sleep_pins_d>;
pinctrl-2 = <&usart2_idle_pins_d>;
status = "okay";
};
in the .dts.
I added this part also in the dts of the tf-a project.
Then i generated the fip bianary file. When flashing, I see cubeprogrammer Logs on usart2.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-12 8:57 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-14 11:55 PM
@Lmoio.1 I did not write that, but my dts has the same descriptions/settings for the usart1 pins:
&usart1{
u-boot,dm-pre-reloc;
pinctrl-names = "default", "sleep";
pinctrl-0 = <&usart1_pins_z_mx>;
pinctrl-1 = <&usart1_sleep_pins_z_mx>;
status = "okay";
};
and for the pinmux section:
&pinctrl_z {
u-boot,dm-pre-reloc;
usart1_pins_z_mx: usart1_mx-0 {
pins1 {
u-boot,dm-pre-reloc;
pinmux = <STM32_PINMUX('Z', 6, AF7)>; /* USART1_RX */
bias-disable;
};
pins2 {
u-boot,dm-pre-reloc;
pinmux = <STM32_PINMUX('Z', 7, AF7)>; /* USART1_TX */
bias-disable;
drive-push-pull;
slew-rate = <0>;
};
};
usart1_sleep_pins_z_mx: usart1_sleep_mx-0 {
u-boot,dm-pre-reloc;
pins {
pinmux = <STM32_PINMUX('Z', 6, ANALOG)>, /* USART1_RX */
<STM32_PINMUX('Z', 7, ANALOG)>; /* USART1_TX */
};
};
};
Actually, STM32CubeMX does not include any _idle sections as yours, but I think it's not an issue. Using the following config for build u-boot:
CONFIG_DEBUG_UART=y
CONFIG_DEBUG_UART_BASE=0x5C000000
CONFIG_LOG=y
CONFIG_LOG_CONSOLE=y
CONFIG_SPL_LOG=y
CONFIG_SPL_LOG_CONSOLE=y
and modifying accordingly the spl.c file to be adapted for usart1, I can clearly see the output in my serial terminal, so I suppose it's not a serial issue, but something else. Clocks? Initialization? During relocation?
Any ideas?
Regards,
Gianluca
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 12:31 AM
Hi,
have you added in the tf-a dts the following:
DECPROT(STM32MP1_ETZPC_USART1_ID, DECPROT_NS_RW, DECPROT_UNLOCK).
Maybe it could be a problem related to GPIOZ pins assigned to the secure context? Can you post your log?
Lidia
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-11-15 5:50 AM
I am not using TF-A, just normal SPL & u-boot load fsbl1 & fsbl2 and ssbl.
Is there any chance on JTAG debugging without having boot from SD Card? Just to know if there is a quick way to check whats happening.
I tried with openocd and gdb, and having break points in _start and _main it hangs on a cpu.c where security_init manage some busy loop tests. If I commented out the security_init, it crashes with undefined instruction in the update_bootmode() function.
I am very close to have a running custom board with it, but it is hard to find out what's going on. Anyway the low level serial output *IS ON THE RIGHT USART1* as I am seeing it crashing and resetting. So I suppose something about the relocation of the device-tree or not so well initialized device-tree structure in static RAM.
If I compile the u-boot & spl for STM32MP157C-DK2 (the EVK I own) it runs very good. And the differences are very little:
- CPU 157C instead of 151A
- DeviceTree wise the pin, clocks configuration nodes are naturally different,
- All the rest of code is identical
The devicetree from my point-of-view is automatically generated by STMCubeMX (latest version as today's) and the u-boot,dm-pre-reloc are in every node I need to use in the SPL.
Here is the configuration I am using in u-boot 2021-01-rc1:
CONFIG_ARM=y
CONFIG_ARCH_STM32MP=y
CONFIG_SYS_MALLOC_F_LEN=0x3000
CONFIG_SYS_MEMTEST_START=0xc0000000
CONFIG_SYS_MEMTEST_END=0xc4000000
CONFIG_ENV_OFFSET=0x280000
CONFIG_ENV_SECT_SIZE=0x40000
CONFIG_SPL_DM_SPI=y
CONFIG_DEFAULT_DEVICE_TREE="stm32mp151a-ek440-mx"
CONFIG_SPL_TEXT_BASE=0x2FFC2500
CONFIG_SPL_MMC=y
CONFIG_SPL=y
CONFIG_TARGET_ST_STM32MP15x=y
CONFIG_CMD_STM32KEY=y
CONFIG_CMD_STM32PROG=y
CONFIG_ENV_OFFSET_REDUND=0x2C0000
CONFIG_TYPEC_STUSB160X=y
CONFIG_SPL_SPI_FLASH_SUPPORT=y
CONFIG_SPL_SPI=y
# CONFIG_ARMV7_VIRT is not set
CONFIG_DISTRO_DEFAULTS=y
CONFIG_SYS_LOAD_ADDR=0xc2000000
CONFIG_FIT=y
CONFIG_BOOTDELAY=1
CONFIG_BOOTCOMMAND="run bootcmd_stm32mp"
CONFIG_SPL_LOG=y
CONFIG_BOARD_EARLY_INIT_F=y
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_USE_PARTITION=y
CONFIG_SYS_MMCSD_RAW_MODE_U_BOOT_PARTITION=3
CONFIG_SPL_ENV_SUPPORT=y
CONFIG_SPL_I2C=y
CONFIG_SPL_MTD_SUPPORT=y
CONFIG_SPL_DM_SPI_FLASH=y
CONFIG_SPL_POWER=y
CONFIG_SPL_SPI_FLASH_MTD=y
CONFIG_SYS_SPI_U_BOOT_OFFS=0x80000
CONFIG_SYS_PROMPT="STM32MP> "
CONFIG_CMD_ADTIMG=y
CONFIG_CMD_ERASEENV=y
CONFIG_CMD_NVEDIT_EFI=y
CONFIG_CMD_MEMINFO=y
CONFIG_CMD_MEMTEST=y
CONFIG_CMD_UNZIP=y
CONFIG_CMD_ADC=y
CONFIG_CMD_CLK=y
CONFIG_CMD_DFU=y
CONFIG_CMD_FUSE=y
CONFIG_CMD_GPIO=y
CONFIG_CMD_I2C=y
CONFIG_CMD_MMC=y
CONFIG_CMD_REMOTEPROC=y
CONFIG_CMD_SPI=y
CONFIG_CMD_USB=y
CONFIG_CMD_USB_MASS_STORAGE=y
CONFIG_CMD_BMP=y
CONFIG_CMD_CACHE=y
CONFIG_CMD_EFIDEBUG=y
CONFIG_CMD_TIME=y
CONFIG_CMD_RNG=y
CONFIG_CMD_TIMER=y
CONFIG_CMD_PMIC=y
CONFIG_CMD_REGULATOR=y
CONFIG_CMD_EXT4_WRITE=y
CONFIG_CMD_MTDPARTS=y
CONFIG_CMD_LOG=y
CONFIG_CMD_UBI=y
# CONFIG_SPL_DOS_PARTITION is not set
CONFIG_OF_LIVE=y
CONFIG_OF_SPL_REMOVE_PROPS="interrupts interrupt-names interrupts-extended interrupt-controller \\\#interrupt-cells interrupt-parent dmas dma-names assigned-clocks assigned-clock-rates assigned-clock-parents hwlocks"
CONFIG_ENV_IS_NOWHERE=y
CONFIG_ENV_IS_IN_MMC=y
CONFIG_ENV_IS_IN_SPI_FLASH=y
CONFIG_ENV_IS_IN_UBI=y
CONFIG_SYS_REDUNDAND_ENVIRONMENT=y
CONFIG_ENV_UBI_PART="UBI"
CONFIG_ENV_UBI_VOLUME="uboot_config"
CONFIG_ENV_UBI_VOLUME_REDUND="uboot_config_r"
CONFIG_SYS_RELOC_GD_ENV_ADDR=y
CONFIG_SYS_MMC_ENV_DEV=-1
# CONFIG_SPL_ENV_IS_NOWHERE is not set
# CONFIG_SPL_ENV_IS_IN_SPI_FLASH is not set
CONFIG_STM32_ADC=y
CONFIG_SET_DFU_ALT_INFO=y
CONFIG_USB_FUNCTION_FASTBOOT=y
CONFIG_FASTBOOT_BUF_ADDR=0xC0000000
CONFIG_FASTBOOT_BUF_SIZE=0x02000000
CONFIG_FASTBOOT_USB_DEV=1
CONFIG_FASTBOOT_FLASH=y
CONFIG_FASTBOOT_FLASH_MMC_DEV=1
CONFIG_FASTBOOT_MMC_BOOT_SUPPORT=y
CONFIG_FASTBOOT_MMC_BOOT1_NAME="mmc1boot0"
CONFIG_FASTBOOT_MMC_BOOT2_NAME="mmc1boot1"
CONFIG_FASTBOOT_MMC_USER_SUPPORT=y
CONFIG_FASTBOOT_MMC_USER_NAME="mmc1"
CONFIG_FASTBOOT_CMD_OEM_FORMAT=y
CONFIG_FASTBOOT_CMD_OEM_PARTCONF=y
CONFIG_FASTBOOT_CMD_OEM_BOOTBUS=y
CONFIG_GPIO_HOG=y
CONFIG_DM_HWSPINLOCK=y
CONFIG_HWSPINLOCK_STM32=y
CONFIG_DM_I2C=y
CONFIG_SYS_I2C_STM32F7=y
CONFIG_LED=y
CONFIG_LED_GPIO=y
CONFIG_DM_MAILBOX=y
CONFIG_STM32_IPCC=y
CONFIG_STM32_FMC2_EBI=y
CONFIG_SUPPORT_EMMC_BOOT=y
CONFIG_STM32_SDMMC2=y
CONFIG_MTD=y
CONFIG_DM_MTD=y
CONFIG_SYS_MTDPARTS_RUNTIME=y
CONFIG_MTD_RAW_NAND=y
CONFIG_NAND_STM32_FMC2=y
CONFIG_SYS_NAND_ONFI_DETECTION=y
CONFIG_MTD_SPI_NAND=y
CONFIG_DM_SPI_FLASH=y
CONFIG_SPI_FLASH_MACRONIX=y
CONFIG_SPI_FLASH_SPANSION=y
CONFIG_SPI_FLASH_STMICRO=y
CONFIG_SPI_FLASH_WINBOND=y
# CONFIG_SPI_FLASH_USE_4K_SECTORS is not set
CONFIG_SPI_FLASH_MTD=y
CONFIG_PHY_REALTEK=y
CONFIG_DM_ETH=y
CONFIG_DWC_ETH_QOS=y
CONFIG_PHY=y
CONFIG_PHY_STM32_USBPHYC=y
CONFIG_PINCONF=y
# CONFIG_SPL_PINCTRL_FULL is not set
CONFIG_PINCTRL_STMFX=y
CONFIG_DM_PMIC=y
# CONFIG_SPL_PMIC_CHILDREN is not set
CONFIG_PMIC_STPMIC1=y
CONFIG_DM_REGULATOR=y
CONFIG_DM_REGULATOR_FIXED=y
CONFIG_DM_REGULATOR_GPIO=y
CONFIG_DM_REGULATOR_STM32_VREFBUF=y
CONFIG_DM_REGULATOR_STPMIC1=y
CONFIG_REMOTEPROC_STM32_COPRO=y
CONFIG_DM_RNG=y
CONFIG_RNG_STM32MP1=y
CONFIG_DM_RTC=y
CONFIG_RTC_STM32=y
CONFIG_SERIAL_RX_BUFFER=y
CONFIG_SPI=y
CONFIG_DM_SPI=y
CONFIG_STM32_QSPI=y
CONFIG_STM32_SPI=y
CONFIG_USB=y
CONFIG_DM_USB_GADGET=y
CONFIG_USB_EHCI_HCD=y
CONFIG_USB_EHCI_GENERIC=y
CONFIG_USB_GADGET=y
CONFIG_USB_GADGET_MANUFACTURER="STMicroelectronics"
CONFIG_USB_GADGET_VENDOR_NUM=0x0483
CONFIG_USB_GADGET_PRODUCT_NUM=0x5720
CONFIG_USB_GADGET_DWC2_OTG=y
CONFIG_DM_VIDEO=y
CONFIG_BACKLIGHT_GPIO=y
CONFIG_VIDEO_LCD_ORISETECH_OTM8009A=y
CONFIG_VIDEO_LCD_RAYDIUM_RM68200=y
CONFIG_VIDEO_STM32=y
CONFIG_VIDEO_STM32_DSI=y
CONFIG_VIDEO_STM32_MAX_XRES=1280
CONFIG_VIDEO_STM32_MAX_YRES=800
CONFIG_VIDEO_BMP_RLE8=y
CONFIG_BMP_16BPP=y
CONFIG_BMP_24BPP=y
CONFIG_BMP_32BPP=y
CONFIG_WDT=y
CONFIG_WDT_STM32MP=y
CONFIG_ERRNO_STR=y
CONFIG_FDT_FIXUP_PARTITIONS=y
# CONFIG_LMB_USE_MAX_REGIONS is not set
CONFIG_LMB_MEMORY_REGIONS=2
CONFIG_LMB_RESERVED_REGIONS=16
CONFIG_DEBUG_UART=y
CONFIG_DEBUG_UART_STM32=y
CONFIG_DEBUG_UART_BASE=0x5C000000
CONFIG_LOG=y
CONFIG_LOG_CONSOLE=y
CONFIG_SPL_LOG=y
CONFIG_SPL_LOG_CONSOLE=y
Can anybody out-there give me an hint on to proceed further?
Regards,
Gianluca