cancel
Showing results for 
Search instead for 
Did you mean: 

Can't boot from SD card on STM32MP157A-EV1

CC
Associate II

I am trying to get this board up and running again after being away from it for a while, but I've been running into problems trying to boot from the SD card. I followed the instructions from the wiki here: https://wiki.st.com/stm32mpu/wiki/STM32MP15_Evaluation_boards_-_Starter_Package

I tried flashing in DFU mode:

~/Downloads/stm32mp1-openstlinux-5.4-dunfell-mp1-20-06-24/images/stm32mp1$ STM32_Programmer_CLI -tm 20000 -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157a-ev1-trusted.tsv 
      -------------------------------------------------------------------
                        STM32CubeProgrammer v2.5.0                  
      -------------------------------------------------------------------
 
 
 
Warning: Timeout is forced to 20000 ms
 
 
USB speed   : High Speed (480MBit/s)
Manuf. ID   : STMicroelectronics
Product ID  : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN          : 003E003E3438511638333630
FW version  : 0x0110
Device ID   : 0x0500
Device name : STM32MP1
Device type : MPU
Device CPU  : Cortex-A7
 
 
Start Embedded Flashing service
 
 
 
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157a-ev1-serialboot.stm32
  File          : tf-a-stm32mp157a-ev1-serialboot.stm32
  Size          : 241984 Bytes
  Partition ID  : 0x01 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:00.634
 
RUNNING Program ... 
  PartID:      :0x01 
Start operation done successfully at partition 0x01
 
Flashlayout Programming ...
[==================================================] 100% 
Running Flashlayout Partition ...
Flashlayout partition started successfully
 
 
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157a-ev1-trusted.stm32
  File          : u-boot-stm32mp157a-ev1-trusted.stm32
  Size          : 874861 Bytes
  Partition ID  : 0x03 
 
Download in Progress:
[==================================================] 100% 
 
File download complete
Time elapsed during download operation: 00:00:01.154
 
RUNNING Program ... 
  PartID:      :0x03 
 
reconnecting the device ...
 
Error: 
Unable to reconnect the target device: time out expired
 
 
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed

I have also tried populating the SD card directly with dd, the results:

NOTICE:  CPU: STM32MP157AAA Rev.B                                               
NOTICE:  Model: STMicroelectronics STM32MP157A eval daughter on eval mother     
NOTICE:  Board: MB1263 Var1.0 Rev.C-01                                          
INFO:    Reset reason (0x15):                                                   
INFO:      Power-on Reset (rst_por)                                             
INFO:    PMIC version = 0x10                                                    
INFO:    Using SDMMC                                                            
INFO:      Instance 1                                                           
INFO:    Boot used partition fsbl1                                              
ERROR:   stm32_sdmmc2_read: timeout 1s (status = 81000)                         
INFO:    SDMMC_POWER    = 0x13                                                  
INFO:    SDMMC_CLKCR    = 0x134002                                              
INFO:    SDMMC_ARGR     = 0xfffff1                                              
INFO:    SDMMC_CMDR     = 0x146                                                 
INFO:    SDMMC_RESPCMDR = 0x6                                                   
INFO:    SDMMC_RESP1R   = 0x900                                                 
INFO:    SDMMC_RESP2R   = 0x0                                                   
INFO:    SDMMC_RESP3R   = 0x0                                                   
INFO:    SDMMC_RESP4R   = 0x0                                                   
INFO:    SDMMC_DTIMER   = 0xffffffff                                            
INFO:    SDMMC_DLENR    = 0x40                                                  
INFO:    SDMMC_DCTRLR   = 0x62                                                  
INFO:    SDMMC_DCNTR    = 0x40                                                  
INFO:    SDMMC_MASKR    = 0x0                                                   
INFO:    SDMMC_ACKTIMER = 0x0                                                   
ERROR:   stm32_sdmmc2_send_cmd_req: CTIMEOUT (cmd = 12,status = 804)            
WARNING:  CMD12, Retry: 0, Error: -60                                           
ERROR:   stm32_sdmmc2_send_cmd_req: CTIMEOUT (cmd = 12,status = 804)            
WARNING:  CMD12, Retry: 1, Error: -60                                           
ERROR:   stm32_sdmmc2_send_cmd_req: CTIMEOUT (cmd = 12,status = 804)            
WARNING:  CMD12, Retry: 2, Error: -60                                           
ERROR:   stm32_sdmmc2_send_cmd_req: CTIMEOUT (cmd = 12,status = 804)            
WARNING:  CMD12, Retry: 3, Error: -60                                           
ERROR:   SDMMC1 init failed                                                     
PANIC at PC : 0x2ffd7911                                                        
                                                                                
Exception mode=0x00000016 at: 0x0000f289

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Olivier GALLIEN
ST Employee

Hi @CC​ ,

Very weird and unusual issue ...

Could you share SDCard memory model you are using ?

Do you have a chance to try with another one ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
CC
Associate II

Hi @Community member​ , thanks for looking into this.

I have tried a SanDisk Edge 16 GB Class 10, SanDisk Ultra 32 GB SDHC Class 10, and a Kingston 8 GB Class 4, all with the same results.

PatrickF
ST Employee

Hi,

Could you share precise boards references and serial number ?

To confirm if there is a undetected regression in our deliveries, could you give a try with the previous starter package ?

e,g, selecting v1.2.0 on this link :https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1starter.html#get-software

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

@PatrickF​ 

I tried v1.2.0 and v1.0.0, same results.

I'm not exactly sure where to find board reference number and serial number, I don't have the original packaging with me at the moment (I can get it if necessary). Hopefully this picture captures it? Thanks0693W0000059ChyQAE.jpg

PatrickF
ST Employee

Please check carefully that all jumpers are set to their default (according to board UserManual).

Maybe worth to try to Flash and Boot using embedded eMMC.

Sound very strange that board is partially booting, you might have a weird HW issue around the SD-Card. BootROM and first level boot are using 1-bit data, then 4-bit data is used at one point of time, which might explain that the boot is starting ok then failing.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.