Skip to main content
Visitor II
May 5, 2025
Question

Problem updating HDMI resolution on STM32MP157F-DK2 (LT6711A + IPS Mono LCD)

  • May 5, 2025
  • 1 reply
  • 426 views

 

Hi,

I'm trying to change the HDMI output resolution of my STM32MP157F-DK2 board to support a BOE 13.3" Mono IPS LCD (connected via LT6711A HDMI to eDP bridge).

What I’ve done so far:

  1. Extracted and edited the device tree source:

    • Decompiled stm32mp157f-dk2.dtb using dtc -I dtb -O dts.

    • Modified display-timings node to match my panel:

      dts
      CopyEdit
      timing0: timing0 { clock-frequency = <74250000>; // or appropriate pixel clock hactive = <1280>; vactive = <720>; hfront-porch = <110>; hback-porch = <220>; hsync-len = <40>; vfront-porch = <5>; vback-porch = <20>; vsync-len = <5>; hsync-active = <0>; vsync-active = <0>; de-active = <1>; pixelclk-active = <0>; };
  2. Recompiled the DTS to DTB:

    • Used: dtc -I dts -O dtb -o stm32mp157f-dk2.dtb stm32mp157f.dts

  3. Replaced DTB on SD card:

    • Mounted bootfs partition.

    • Copied new stm32mp157f-dk2.dtb to /bootfs/

  4. Updated extlinux.conf:

    • Ensured that FDT /stm32mp157f-dk2.dtb is set correctly in:

      bash
      CopyEdit
      /boot/mmc0_extlinux/extlinux.conf
  5. Verified after boot:

    • Device tree seems to load (checked /proc/device-tree/model and dtb name).

    • But /sys/class/drm/card0-HDMI-A-1/modes still only shows 720x480.


Question:
Despite updating and loading the correct DTB, the HDMI output still defaults to 720x480. Is there a specific step or kernel option I’m missing to make the HDMI resolution switch correctly? Should I define a fixed mode via a hdmi-connector node or change something in the display controller node?

Thanks in advance!

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
May 5, 2025

Hi @nikbakhtfaezeh 

do this helps ?

https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

 

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent