cancel
Showing results for 
Search instead for 
Did you mean: 

Can I include "tf-a-v2.2-stm32mp-r1.3" when making Yocto-based distributions?

Machilus
Associate III

Hi all

I am making a distribution based on "Eco System 2.0.0" and yocto.

I have a problem with TF-A when making a distribution package.

This is the "stm32mp1_clk_get_gated_id: clk id 85 not found" error message from "tf-a-v2.2-stm32mp-r1.0"

I know it's resolved in "tf-a-v2.2-stm32mp-r1.3", but it doesn't apply to yocto yet

I would like to know if there is a way to apply the "tf-a-v2.2-stm32mp-r1.3" version to yocto.

"devtool modify -x tf-a-stm32mp workspace/tf-a"

I used the above command to replace existing source with "r1.3" source and created a distribution, but the version of the "tf-a-xxxxx-serialboot.stm32" file is still "r1.0".

When I download using "STM32CubeProgrammer" I get the same error.

Any answers would be appreciated.

Thanks and regards

Machilus

1 REPLY 1
Machilus
Associate III

I solved the problem by referring to the notice.

However, it seems that the content of how to apply the minor release found by WIKI is too poor.

I think you'd better supplement the content.

Thanks and regards

Machilus