cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN controller disable receive warn interrupt in stm32mp1

Ara.1
Senior

do we have any bit disable particular can frame receive warn message as we have in imx6 platform ?

RWRN_MSK

This bit provides a mask for the Rx Warning Interrupt associated with the RWRN_INT flag in the Error andStatus Register. This bit is read as zero when MCR[WRN_EN] bit is negated. This bit can only be written ifMCR[WRN_EN] bit is asserted.

1Rx Warning Interrupt enabled

0Rx Warning Interrupt disabled

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Hi,

I'm not CAN specialist, but according to RM0436 (STM32MP157 advanced Arm®-based 32-bit MPUs), there is in FDCAN_IE (together with many other interrupt enable bits)

Bit 24 EWE: Warning status interrupt enable

0: Interrupt disabled

1: Interrupt enabled

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Ara.1
Senior

yes i check this flag but it is generic for tx warn and rx warn message.

i try to send miss can baud from can analyser send, expected not to increase any receive warn.