2021-01-20 5:21 PM
We have product built around STM32MP1157C and boots up with GPT partition table. However, we would like to boot it up with DOS (MBR based) Partition table. As per the documentation - section 4.3 of https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview, it seems GPT is not mandatory for STM32 ROM code to locate FSBL. So, accordingly, I dumped u-boot-spl.stm32-mp1som-pxl7-basic at LBA 34 (at offset 17K), but it fails to boot up.
Any help in this regard is highly appreciated.
Thanks,
Pradeep
2021-01-21 1:13 AM
Hi @Community member ,
Can you please confirm you are booting from SDCard ?
Can you describe further "but it fails to boot up" ? Any log trace ?
What is status on PA13 ( see https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Debug_and_Error_messages )
Olivier
2021-01-21 3:48 AM
Hi Olivier,
Thanks for the response.
Yes, I am booting up from SDcard.
By 'fails to boot up', I mean the FSBL never comes up as I don't see any logs on the debug console. However, same FSBL comes up, if I use the gpt partition table.
I haven't checked the status of PA13. I would check & let you know soon.
Thanks,
Pradeep
2021-01-21 8:44 AM
Hi Olivier,
Unfortunately, we don't have pin PA13 directly accessible on the board, neither we have a debugger to get the logs. However, it would be very helpful if you could point me to some instructions which guides on the booting up with non-GPT partition table. This is what I did:
Regards,
Pradeep
2021-02-18 7:23 AM
Hi @Community member ,
It appears that wiki information maybe erroneous.
Bootrom is looking at LBA128 (offset 64KB) for FSBL1 and LBA640 ( offset 320KB) for FSBL2.
Please give it a try.
FYI, MBR support is not integrated in our TF-A trusted boot solution, which is the one recommended.
Basic boot is no longer supported since Version 2.0.
As matter of curiosity what prevent you to use GPT partitioning ?
Thx
Olivier