cancel
Showing results for 
Search instead for 
Did you mean: 

how to join two bytes into a 16-bit float. .

guerrondo
Associate

the microcontroller receives a total of 4 bytes of data every 50 µs via SPI.  each Two bytes form a value,  which is represented as a float with 16 bits.

how can i join two bytes into a 16-bit float?

float v_beta_d_star = 0.0f;

float v_beta_q_star = 0.0f;

float v_beta_d_star = (spi_values[0] << 8) | (spi_values[0] & 0xFF);

float v_beta_d_star = (spi_values[1] << 8) | (spi_values[1] & 0xFF);

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Javier1
Principal

floats have 32 bit, and they dont store data the same way as integers or byte variables.

I dont know if this will help you but:

from two byte variables to one uint16_t;

memcpy(&first16bitvariable,&spi_values[0],2);

memcpy(&second16bitvariable,&spi_values[2],2);

once you have the 16bit integers you can use them to do some maths with floats

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero
Uwe Bonnes
Principal III

Nitpicking:

memcpy does not care for byte order in your spi data. With 16bitvariable = spi_values[0] | spi_values[1] << 8 or 16bitvariable = spi_values[1] | spi_values[0] << 8 you can care for byte order.

Ozone
Principal

Floating point formats are standardized, see here: https://en.wikipedia.org/wiki/IEEE_754

For endianess, check the datasheet of the SPI slave you receive the values from.

Alternatively, the datasheet should define the number format used.