cancel
Showing results for 
Search instead for 
Did you mean: 

STm32CubeMX 6.14 does not copie all library files from package

Jagr
Associate II

Hi,
i updated CubeMX to version 6.14 and therfor update STM32MP1 firmware package to v1.7.0
- STM32Cube FW_MP1 V1.7.0

In my project i am using the Option to copiy only need library files to project

Jagr_0-1741794149398.png

But this does not work correctly.
There are some files, header files, missing under Middlewares\Third_Party\FreeRTOS
The files are all existing in the packge under C:/Users/XYZ/STM32Cube/Repository/STM32Cube_FW_MP1_V1.7.0
but not being copied to Project folder.

Can anybody confirm this issue?

P.s. when i use firmware package 1.6.0 with CubeMX v6.14 everything is fine.

Regards

0 REPLIES 0