cancel
Showing results for 
Search instead for 
Did you mean: 

About "VREF+" pin

tatsuya
Associate II

Hi team,

I am developing our PCB referring to the "STM32MP157 EVAL"(MB1263-C04 Board schematic).

https://www.st.com/en/evaluation-tools/stm32mp157f-ev1.html#cad-resources

In the datasheet, VREF+ looks like a voltage output pin, but why is power supply connected to VREF+ in STM32MP157 EVAL?

Best regard,

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
QSHAO.1
ST Employee

in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.

View solution in original post

4 REPLIES 4
Piranha
Chief II

Maybe read the text in the image you posted?

QSHAO.1
ST Employee

in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.

EZHON.1
ST Employee

Don't forget to add a 1uF capacitor for decoupling when used as output.

PatrickF
ST Employee

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.