2022-12-06 06:31 PM
Hi team,
I am developing our PCB referring to the "STM32MP157 EVAL"(MB1263-C04 Board schematic).
https://www.st.com/en/evaluation-tools/stm32mp157f-ev1.html#cad-resources
In the datasheet, VREF+ looks like a voltage output pin, but why is power supply connected to VREF+ in STM32MP157 EVAL?
Best regard,
Solved! Go to Solution.
2022-12-06 07:25 PM
in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.
2022-12-06 07:06 PM
Maybe read the text in the image you posted?
2022-12-06 07:25 PM
in datasheet, it's mentioned that "An external voltage reference can be provided through the VREF+ pin when the internal voltage reference buffer is off". so external Vref+ mode is used on the board.
2022-12-06 09:48 PM
Don't forget to add a 1uF capacitor for decoupling when used as output.
2022-12-08 12:12 AM
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'