STM32MP157-DK2 can not boot after fuse prog command attempt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-07 3:36 AM
Hello!
How to fix STM32MP1157-DK2:
My board cannot boot after attempt of MAC address changing by fuse programming from U-Boot command line:
fuse prog -y 0 57 0x78563412 0x0000bc9a
Then we got following during boot process:
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
NOTICE: Board: MB1272 Var2 Rev.C-01
INFO: Reset reason (0x10):
INFO: Reset due to a failure of VDD_CORE
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
INFO: Product_below_2v5=1: HSLVEN update is
INFO: destructive, no update as VDD>2.7V
NOTICE: BL2: v2.0(debug):
NOTICE: BL2: Built : 13:13:37, Oct 2 2018
INFO: BL2: Doing platform setup
INFO: PMIC version = 0x10
INFO: RAM: DDR3-1066/888 bin G 1x4Gb 533MHz v1.41
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2fff0000
INFO: Image id=4 loaded: 0x2fff0000 - 0x30000000
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: STM32 Image size : 748404
WARNING: Skip signature check (header option)
INFO: Image id=5 loaded: 0xc0100000 - 0xc01b6b74
INFO: read version 0 current version 0
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2fff0000
INFO: SPSR = 0x1d3
PANIC at PC : 0x2fff6243
Exception mode=0x00000016 at: 0xfffffffc
We tried to fix it by following:
1) attempt to connect by SWD causes error:
09:40:40 : ST-LINK SN : 0672FF353036465043221036
09:40:40 : ST-LINK FW : V2J35M0
09:40:40 : Voltage : 3,21V
09:40:40 : Error: No STM32 target found!
2) attempt to rewrite software by STM32CubeProgrammer and DFU Boot0=off, Boot2=off causes message:
09:48:15 : USB speed : High Speed (480MBit/s)
09:48:15 : Manuf. ID : STMicroelectronics
09:48:15 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
09:48:15 : SN : 002A002B3338510939303435
09:48:15 : FW version : 0x0110
09:48:15 : Device ID : 0x0500
09:48:27 : Read TSV File: /home/user/Downloads/en.FLASH-stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/stm32mp1-openstlinux-4.19-thud-mp1-19-10-09/images/stm32mp1/flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv
09:48:27 : Number of partitions: 9
09:48:36 : Start Embedded Flashing service
09:48:36 : Memory Programming ...
09:48:36 : Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
09:48:36 : File : tf-a-stm32mp157c-dk2-trusted.stm32
09:48:36 : Size : 245364 Bytes
09:48:36 : Partition ID : 0x01
09:48:36 : Download in Progress:
09:48:37 : File download complete
09:48:37 : Time elapsed during download operation: 00:00:00.423
09:48:37 : RUNNING Program ...
09:48:37 : PartID: :0x01
09:48:37 : Start operation done successfully at partition 0x01
09:48:37 : Flashlayout Programming ...
09:48:37 : Running Flashlayout Partition ...
09:48:37 : Flashlayout partition started successfully
09:48:37 : Memory Programming ...
09:48:37 : Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
09:48:37 : File : u-boot-stm32mp157c-dk2-trusted.stm32
09:48:37 : Size : 805514 Bytes
09:48:37 : Partition ID : 0x03
09:48:37 : Download in Progress:
09:48:37 : File download complete
09:48:37 : Time elapsed during download operation: 00:00:00.580
09:48:37 : RUNNING Program ...
09:48:37 : PartID: :0x03
09:48:37 : reconnecting the device ...
09:49:07 : Error: unable to reconnect the target device: time out expired
09:49:08 : Error: Start operation failed at partition 0x03
09:49:08 : Error: TSV flashing service failed
09:49:08 : Warning: Connection to device 0x500 is lost
09:49:08 : Disconnected from device.
Thank you in advance!
BR
Ivan
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-07 4:51 AM
Hello,
reprogramming non-blank One Time Programming fuses such as MAC address make them corrupted as bits can only be set to '1' and as they are protected by an hidden ECC, which is corrupted as well. Only lower OTP (1024 bits) are set to be fuses one by one.
As MAC address read from OTP return a corruption error, this might explain the panic. I will check if it is possible to skip it.
In future batch of STM32MP15x-DK1/DK2 boards, the MAC address would be write protected to avoid such mistake.
Btw, what is the purpose of changing the MAC address ? MAC address on all ST board is already programmed and there is no need to change it.
Only on your own board, with 'blank' STM32MP15x devices, MAC address in your company attributed range should be programmed in OTP.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-07 5:20 AM
Thank you Patrick!
1)How to fix it?
Is it possible to return previous values by erase - burn or somehow else?
2) We use DK2 board for prototyping and need to understand how to process MAC in future mass production according to assigned purchased MAC range.
Regards
Ivan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-07 5:21 AM
You should change the TF-A devicetree to remove bsec mac_address node.
Note: It is then not possible anymore to read the mac address from the OTP (which is anyway corrupted)
With that change, your board should boot, but with an error as MAC address is not set
- the mac address is stored in u-boot env:
STM32MP> env print ethaddr
ethaddr=00:80:e1:42:45:20 (address example)
- So each time you reflash your board, you will need to reinitialize the mac address:
STM32MP> env set ethaddr 00:80:e1:42:45:20 (address example)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-07 8:09 AM
Thank You Patrick!
Regards,
Ivan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-10 1:40 AM
Hello!
How to repair my board, I don't understand how to change the TF-A devicetree on my board, I don't understand what tool is helpful in my case?
Regards,
Ivan
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-10 2:05 AM
Sorry for not being clear .... here are more details:
I/ To modify your TF-A:
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Modifying_the_TF-A
II/ To be able to boot with your corrupted otp (mac_address), you will need to remove:
this node:
&bsec {
mac_addr: mac_addr@e4 {
reg = <0xe4 0x6>;
};
in this file: stm32mp157c-security.dtsi
III/ Then hile booting your board with the new TF-A devicetree, you won't get the boot error
IV/ But your mac address will be invalid, so you may update it in U-boot (u-boot console):
STM32MP> env set ethaddr 00:80:e1:42:45:20 (address example)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-10 7:14 AM
Thank You!
Regards
Ivan