Hello Stefan,
Yes this is the same patch already shared in zip. You need to apply it in Yocto bsp layer (you can use git am or git apply-patch for that) : openstlinux-6.1-yocto-mickledore-mp1-v23.06.21/layers/meta-st/meta-st-stm32mp.
The patch will c...
@debugging, These wiki articles are generic ones ("how to's"). The issue here comes from Arm gcc toolchain version and the patch (consisting in moving to another arm gcc toolchain version) will be integrated in V5.0.1 version delivered today.
But it ...
Yes this is Arm gcc, here is the patch:
diff --git a/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi_11.inc b/recipes-devtools/gcc-arm-none-eabi/gcc-arm-none-eabi_11.incindex 515784a..3d2a65b 100644--- a/recipes-devtools/gcc-arm-none-eabi/gcc-...