2020-10-21 7:42 PM
These are log i got during download, any clue
STM32_Programmer_CLI -c port=usb1 -tm 20000 -w flashlayout_mp1som-image/FlashLayout_sdcard_mp1som-mystm32mp1-basic.tsv
-------------------------------------------------------------------
STM32CubeProgrammer v2.5.0
-------------------------------------------------------------------
USB speed : High Speed (480MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 001F00213438510838333630
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MP1
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-mp1som-pxl7-trusted.stm32
File : tf-a-mp1som-pxl7-trusted.stm32
Size : 245364 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.465
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-mp1som-pxl7-trusted.stm32
File : u-boot-mp1som-pxl7-trusted.stm32
Size : 790180 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:00.666
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
Error:
Unable to reconnect the target device: time out expired
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
This is a coustom build open-st image
On Ubuntu terminal i see following log:
-------------------------build-mp1som/tmp-glibc/deploy/images/mp1som$ dmesg | tail
[30232.038713] usb 1-5: device descriptor read/64, error -71
[30232.274455] usb 1-5: new high-speed USB device number 100 using xhci_hcd
[30232.423922] usb 1-5: New USB device found, idVendor=0483, idProduct=df11
[30232.423933] usb 1-5: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[30232.423940] usb 1-5: Product: DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
[30232.423945] usb 1-5: Manufacturer: STMicroelectronics
[30232.423951] usb 1-5: SerialNumber: 001F00213438510838333630
[30246.952313] usb 1-5: USB disconnect, device number 100
[30248.890048] usb 1-5: new high-speed USB device number 101 using xhci_hcd
[30254.177938] usb 1-5: device descriptor read/64, error -110
--------------~build-mp1som/tmp-glibc/deploy/images/mp1som$ dmesg | tail
[30290.893477] usb usb1-port5: attempt power cycle
[30291.545421] usb 1-5: new high-speed USB device number 103 using xhci_hcd
[30296.801391] xhci_hcd 0000:00:14.0: Timeout while waiting for setup device command
[30302.177296] xhci_hcd 0000:00:14.0: Timeout while waiting for setup device command
[30302.385249] usb 1-5: device not accepting address 103, error -62
[30302.513257] usb 1-5: new high-speed USB device number 104 using xhci_hcd
[30307.557111] xhci_hcd 0000:00:14.0: Timeout while waiting for setup device command
[30312.929409] xhci_hcd 0000:00:14.0: Timeout while waiting for setup device command
[30313.137046] usb 1-5: device not accepting address 104, error -62
[30313.137099] usb usb1-port5: unable to enumerate USB device
if i connect a fresh sd card 16 GB and create a bootable image using DD, Board boots successfully.
2020-10-22 12:45 AM
Hello Ara.1,
We also face this issue when using ST-DK2 (discovery kit). We don't know what the real cause, but we have this problem on a inux laptop and this issue doesnt appear on another linux pc.
First, i suggest you to try to update (=try to use STM32_Programmer_CLI with) the DK2 starter kit on a dk2 board (you have one isnt it?)
If its ok, do the same with your board.
If not , try another PC, usb cable, usb power and all related "connection" things
good luck
2020-10-22 2:45 AM
May I suggest to read those FAQ:
https://community.st.com/s/article/FAQ-STM32MP1-Bring-up-procedure
also one common pitfall when building your own board is around HSE settings. The BootROM has automatic HSE detection (oscillator or crystal) whereas this setting is fixed in device tree (thus making uBoot stopping to work as it could killing its clock). Our board are using digital bypass with external oscillator (and so our default DT).
please have a look to https://wiki.st.com/stm32mpu/wiki/Clock_device_tree_configuration_-_Bootloader_specific#DT_configuration_for_HSE
2020-10-22 9:02 AM
whats the ubuntu version you used , where it was working ???
2020-10-22 11:49 PM
ubuntu 16.04
do you have the same issue with restoring DK2 stater kit?
do you work on custom board?
2020-10-23 12:25 AM
2020-10-23 1:01 AM
Ah Custom board, ok, i'm sorry, ive no hint anymore, there is too much possibility of mistake.
wish you good luck!
2021-07-20 6:32 AM
In the meantime I have noticed that even more garbage is created if I leave the "/ CS" signal in the new site "Low" state for the entire time a command is processed (sending and receiving)!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.