cancel
Showing results for 
Search instead for 
Did you mean: 

USB DETECTION IN UBOOT-V2023.10

Srikanth1
Senior

Hello

We are Working on a custom board with STM32MP157AAA3 processor.We are using uboot(V2023.10) for checking USB 2nd Port.

we referred the below link to configure the dts :

https://wiki.st.com/stm32mpu/wiki/USBPHYC_device_tree_configuration 

We are using the same dts configuration in uboot(V2023.10) and linux(V5.13),It works in linux but not in uboot.

We are attaching the dts file below.Hope you could refer and suggest us where we are going wrong.

Srikanth1_1-1717401564854.png

 

Thanks&Regards

Srikanth.R

 

 

 

2 REPLIES 2
Christophe Guibout
ST Employee

Hello @Srikanth1,

 

Could you please elaborate a bit more in the problem description (use case description, logs when it doesn't work....) ?

You mentionned using kernel-5.13 : which Ecosystem version do you use ?

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @Christophe Guibout,

 

Thanks for the reply. We are using Buildroot: 2023.08.2

 

 

 

Thanks&Regards

Srikanth.R