2020-05-09 03:27 AM
Hi
dear engineers,
i can run linux on stm32f429 mcu without any problem, but it failed on Cortex-M MCU in stm32mp157 board.
After many hours i realize:
error happens in below function
void __meminit __free_pages_bootmem...
Anyone else had a similar problem? how you resolved it?
Shall i change any register address in kernel? (i think every thing is the same in cortex-M4 and stm32f429).
Best regards
2020-05-11 12:06 AM
Hi @Fheid.1
I supposed you mention STM32F429IDISCO for F4 platform supporting Linux ?
It has 2MB flash while you only have a budget of 384KB of MCU RAM in STM32MP1.
Did you shape your linux system to fit in this space ?
Olivier
2020-05-11 09:00 PM
Hi dear @Community member
Thanks for your attention
Yes you supposed right, I know running linux on cortex M is unusual project.
I have taken the first steps of the project and I hope to do it successfully with your help.
You know better than me the electronic circuit and the structure of stm32mp157,
I use 64 kB and three 128 kB memory in addition to DDR3 for running linux. It is so complex but I can explain it step by step if you want.
After too many ties i can access the attachment picture, Could you understand my recent status using sending image?
Could you help me?
Kind regards
2020-05-11 11:37 PM
Hi @Fheid.1
>> I use 64 kB and three 128 kB memory in addition to DDR3 for running linux
Are you aware that on STM32MP15x, Cortex-M4 is not intended to access DDR content. Cortex-M4 has no cache and asynchronous path to AXI bus has not been optimized for that, so Cortex-M4 performance will be very largely impacted.
I also presume you are running "engineering" mode where DDR3 is not available, since not powered nor configured.
Olivier
2020-05-12 02:19 AM
Hi Mr @Community member
Thank you indeed.
I am running "production" mode and accessing DDR3 is available for me.
Im not worried a bout performance or running speed.
according to RM0436 datasheet i can access to DDR content without any problem.
i have done the following settings on Cortex-A and Cortex-M. please check attached file...
if it is hardly readable tell me to send each of them separately.
2020-05-12 02:31 AM
i mentioned it :
"error happens in below function
void __meminit __free_pages_bootmem..."
i dont know any thing a bout mentioned function. Does that function error occur in a particular situation?