Hi,
I have built the OpenSTLinux distribution according to your wiki guide (https://wiki.st.com/stm32mpu/index.php/STM32MP1_Distribution_Package#Building_the_OpenSTLinux_distribution).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-08 7:38 AM
I want to populate the distribution to an SD-card and mount it in STM32MP157A-DK1 according to this link: https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#How_to_populate_a_microSD_card_inserted_in_a_Linux_host_PC
My host PC is a virtual machine and it seems like there is a problem with STM32CubeProgrammer reconnecting to the device (see uploaded image). I have changed the USB settings on my virtual machine to automatically attach the device to it. This works fine when I press the reset button on STM32MP157A-DK1, it unmounts and mounts directly to the virtual machine again.
How can I solve the reconnecting problem with STM32CubeProgrammer? Is there another way to populate an SD card by copying files from the deploy folder in the built distribution folder?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-08 7:51 AM
Hi, did the flashload work with pre-built Starter Package ?
Otherwise please have a look to https://community.st.com/s/article/FAQ-STM32MP1-STM32CubeProgrammer-USB-reconnect-error-at-STM32MP1-boot-device-flashing
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-13 11:56 PM
No, it didn't.
I have tried to do this on Windows instead and the same problem occurs despite not using a virtual machine. Here is the log from CubeProgrammer:
08:23:31 : Read TSV File: C:\Work\Starter-Package\stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31\images\stm32mp1\flashlayout_st-image-weston\trusted\FlashLayout_sdcard_stm32mp157a-dk1-trusted.tsv
08:23:31 : Number of partitions: 9
08:23:50 : USB speed : High Speed (480MBit/s)
08:23:50 : Manuf. ID : STMicroelectronics
08:23:50 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
08:23:50 : SN : 003000443338510D39303435
08:23:50 : FW version : 0x0110
08:23:50 : Device ID : 0x0500
08:23:54 : Start Embedded Flashing service
08:23:54 : Memory Programming ...
08:23:54 : Opening and parsing file: tf-a-stm32mp157a-dk1-usb.stm32
08:23:54 : File : tf-a-stm32mp157a-dk1-usb.stm32
08:23:54 : Size : 225572 Bytes
08:23:54 : Partition ID : 0x01
08:23:54 : Download in Progress:
08:23:55 : File download complete
08:23:55 : Time elapsed during download operation: 00:00:00.387
08:23:55 : RUNNING Program ...
08:23:55 : PartID: :0x01
08:23:55 : Start operation done successfully at partition 0x01
08:23:55 : Flashlayout Programming ...
08:23:55 : Running Flashlayout Partition ...
08:23:55 : Flashlayout partition started successfully
08:23:55 : Memory Programming ...
08:23:55 : Opening and parsing file: fip-stm32mp157a-dk1-trusted.bin
08:23:55 : File : fip-stm32mp157a-dk1-trusted.bin
08:23:55 : Size : 1064414 Bytes
08:23:55 : Partition ID : 0x03
08:23:55 : Download in Progress:
08:23:56 : File download complete
08:23:56 : Time elapsed during download operation: 00:00:00.957
08:23:56 : RUNNING Program ...
08:23:56 : PartID: :0x03
08:23:56 : Reconnecting the device ...
08:24:26 : Error: Unable to reconnect the target device: time out expired
08:24:26 : Error: Start operation failed at partition 0x03
08:24:26 : Error: TSV flashing service failed
08:24:26 : Warning: Connection to device 0x500 is lost
08:24:26 : Disconnected from device.
What am I doing wrong?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-14 3:13 AM
Hi,
in W10 Device Manager, please check the USB 'DFU in HS mode @...." device properties details.
Property 'Bus reported device description' should be:
- "DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000" when it is issued from the BootROM (used to load partition Id 0x01 and 0x03) after reset with BOOT pin set to 'Serial USB'
- "USB download gadget@Device ID /0x500, @Revision ID /0x2000, @Name /STM32MP157AAC Rev.B," or similar when uBoot is connected (after "Reconnecting the device ..." )
If not, you might have missed some USB driver during installation or some USB devices are disabled (e.g. still point to a Virtual Machine).
Be sure to try with latest CubeProgrammer v2.7.0 and pre-built images from latest Starter Package.
Logging console could help (UART VCP on ST-Link port, 115200,n,8,1)
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-14 3:57 AM
Hi,
The USB in Device Manager is "DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000".
I'm not sure if the DFU driver was installed during installation. STM32 Bootloader.bat file executes without errors but
"PC $> STM32_Programmer_CLI -l usb"
returns:
"STM32_Programmer_CLI : The term 'STM32_Programmer_CLI' is not recognized as the name of a cmdlet, function, script
file, or operable program. Check the spelling of the name, or if a path was included, verify that the path is correct
and try again.
At line:1 char:1
+ STM32_Programmer_CLI -l usb
+ ~~~~~~~~~~~~~~~~~~~~
+ CategoryInfo : ObjectNotFound: (STM32_Programmer_CLI:String) [], CommandNotFoundException
+ FullyQualifiedErrorId : CommandNotFoundException"
I'm using the latest CubeProgrammer and pre-built image from latest Starter Package.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-14 4:58 AM
Please carefully check the property 'Bus reported device description' for point 1 and 2 in my previous reply
When uBoot start, it should be like that (captured from DK2-F):you could also use:
"%ProgramFiles%\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -l usb
and check "Product ID" before flashing (with BootROM DFU) and during Flashing (with uBoot DFU).
Have your tried on another PC or using another USB high-speed port on the PC ?
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-18 5:31 AM
I also faced the similar issue of reconnecting with STM32CubeProgrammer while working on my new page project If there is a possibility to solve this issue then please guide me.