2022-08-26 12:34 AM
Greetings !
I am trying to build stand alone u-boot for my "stm32f769 discovery board". But when I initiate make command I am getting the below error .
Please help me out to resolve this issue.
Error log:
----------------------------------------------------------------------------------------------------------------
user@user-Latitude-3490:~/study/u-boot/u-boot$ make
make[1]: Entering directory '/home/user/study/u-boot/u-boot/stm32f769-disco'
GEN ./Makefile
scripts/kconfig/conf --syncconfig Kconfig
CHK include/config.h
CFG u-boot.cfg
cc1: error: unrecognized command line option "-mno-unaligned-access"
cc1: error: unrecognized command line option "-std=gnu11"
make[2]: *** [../scripts/Makefile.autoconf:77: u-boot.cfg] Error 1
make[1]: *** No rule to make target 'include/config/auto.conf', needed by 'include/config/uboot.release'. Stop.
make[1]: Leaving directory '/home/user/study/u-boot/u-boot/stm32f769-disco'
make: *** [Makefile:167: sub-make] Error 2
---------------------------------------------------------------------------------------------------------------------------
Thanks in Advance
2022-10-03 3:24 AM
Hi,
it seens the cross-compiler ARMv7 is not defines or not installed....
do you have selected the U-Boot configuration (make <board>_defconfig) ?
for compelte steps, see the latest documentation:
https://u-boot.readthedocs.io/en/latest/board/st/stm32_MCU.html
generated from doc/board/st/stm32_MCU.rst
Patrick