Hi, WIKI describes the procedure for actual version of OpenSTlinux we change the sequence on new product STM32MP13 and we align this sequence for STM32MP15 to simplify the management of the DFU stack in bootloaders (in TF-A):U-Boot load himself the f...
Hi,UUID of the GPT partitions are used in TF-A to select the FIP partitions, these UUID information is used in "metadata" used of TFA secure udpate as decrivbe in https://wiki.st.com/stm32mpu/wiki/Secure_Firmware_UpdateYou need also to select the cor...
Hi,your problem is caused by the STM32CubeProgrammer reconnection after U-Boot start:1/ on U-Boot start, the USB stack is started with DFU configuration to request the FlashLayout file (Phase 0x0)2/ on Host side, the STM32Programmer try to access the...
Hi, When I check your trace,the stm32prog command in U-Boot start the USB gadget stack andwait the falshlayout file normally sent by the programmer. But this file is not sent that it is normal if Host don't see the expected DFU USB after enumeration...
Hi,in your trace, it seems the OP-TEE in loaded at address: 0xc6200000INFO: Loading image id=22 at address 0xc6200000INFO: Image id=22 loaded: 0xc6200000 - 0xc624d000And U-Boot use the end of DDR (128 MiB) for relocation address with "Ram top: C80000...