cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong pin configuration for USART1 (Half-Duplex) - STM32WB55

pierpaolo
Associate II

When I use the IDE to configure USART1 in Half-Duplex mode, the GPIO setting is wrong.

Indeed, PB7 is set instead of PB6.

Also, its mode is set to GPIO_MODE_AF_PP instead of GPIO_MODE_AF_OD.

This cannot be changed from the IDE/MX configuration wizard, unfortunately.

0 REPLIES 0