STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

I have gone through the course pre-requisites but have some queries. I cannot communicate to the STM32WL55 via comm port which is preventing me from making progress ahead of the course. Full details listed below, many thanks in advance for you support.

I have started to go through the course pre-requisites and am familiarising myself with the kit and feeling much more confident, particularly as I have the gateway setup on TTN an seeing the L073RZ dev board ping in. I am still going through the prer...

JAshl.1 by Associate
  • 1668 Views
  • 2 replies
  • 0 kudos

STM32WB BLE and USB simultaneous working problem

Hi,​Im using STM32WB55 USB dongle board​. I want to send data from the dongle board to PC using USB pheriperal. i used the command CDC_Transmit() to send data and I visualized the recieved data using realterm in PC . ​I​t was working. But I want to...

SChan.8 by Associate II
  • 791 Views
  • 0 replies
  • 1 kudos

STM32WB55 Memory Layout

Hi,I am new to the STM32WB range. I need to use the 1MB flash version in a project, But I am struggling a bit to understand the flash layout.I read that the first 6 Sectors are to be used my the OTA application. It seems like settings should go direc...

ROost.1 by Associate
  • 804 Views
  • 0 replies
  • 0 kudos

STM32 UART HAL and LL failed

Sorry ST guys but the UART HAL and LL_HAL ist a total fail!I developing over 15 years all kind of serial communication with linux and different microcontrollers. Now I regret my desistion to use the STM32WB MCU. I'm trying over two weeks the get a st...

STUser21 by Associate II
  • 4352 Views
  • 9 replies
  • 0 kudos

ST bluenrg2 low power current consumption

I am developing a Beacon model application with ST bluetile. Bluenrg2 low power current consumption differs between SensorDemo (200uA) and Beacon application (1.8mA). I made sure that the bluetile goes into SLEEP_NO_TIMER mode and wakes up only when ...

SMano by Associate II
  • 703 Views
  • 0 replies
  • 0 kudos