2019-11-18 06:23 PM
I'm using ST-LINK of p-nucleo-wb55 board.
I tried to connect P-Nucleo-wb55 to the ST-LINK Utility, but I can't.
Below the comment of ST-LINK Utility.
11:09:19 : ST-LINK SN : 0671FF393738425043066025
11:09:19 : ST-LINK Firmware version : V2J35M26
11:09:19 : Connected via SWD.
11:09:19 : SWD Frequency = 4,0 MHz.
11:09:19 : Connection mode : Normal.
11:09:19 : Debug in Low Power mode enabled.
11:09:20 : Can not connect to the target!
Please select "Connect Under Reset" mode from Target->Settings menu and try again.
11:09:22 : Unexpected error
When I using the STM32CubeIDE Debug, it works.
But I want to erase the program of wb55.
Can I erase the program on the STM32CubeIDE?
or How can i connect the ST-LINK Utility to P-Nucleo-WB55?
2019-11-19 02:07 AM
Did you try ""Connect Under Reset" ?
2019-11-19 02:31 AM
Yes of course.
I tried every optiongg changed.
2019-11-19 04:05 AM
Did you have a look at AN5185?