cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the "Debug Authentication" ?

MQi.1
Senior II

I used a MB2032-WB09-B02 on MB1801D for several times, flash in CubeIDE was always OK, though debug prompted error read data every time, then the next day when I used it again, it didn't work, I couldn't flash image into neither in IDE nor Prog, the prompt:

 

Screenshot from 2024-12-12 11-23-57.png

 

my question is: how to discovery using Debug Authentication?

3 REPLIES 3
Imen.D
ST Employee

Hello @MQi.1 ,

Check the solder-bridges and jumpers positions (JP2 ON, JP1 on USB_STLK [1-2] on the MB1801 board.)

Switch SW1 should be on the 3V3 power supply (switch on position [1-2]) on the MB1801 board.

Make sure to follow the settings described in the UM3345 STM32WB09 Nucleo-64 board (MB1801 and MB2032) in Getting started section and Table 12. Solder bridges for MB1801.

 

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

In page 9 of "UM3345 STM32WB09 Nucleo-64 board (MB1801 and MB2032)", when MB2032 is upper (Type-C under Reset key), JP1 is on [1, ?], this the default location when I got this board kit (MB1801 + MB2032), while the note is "5V_STLK" not "USB_STLK", and there is also a "VBUS_STLK" on right side, is that right ? I mean is there an error in UM3345 ? Since when I could flash before, I have never find the board before Bluetooth pairing stably, I changed the TX power to MAX (0x1F) as it was told here - page 167 of AN5207 (Tx power level).

I identified the settings described in UM3345, the first 2 items is OK, for item 3 and 5, I didn't use ST Bluetooth® Low Energy sensor mobile application on a Bluetooth® Low Energy compatible mobile device from the App Store or Google Play, I just turn on Bluetooth on the mobile phone and want to find the WB09KE, did this matter?