WB55 Nucleo always drops to Default_Handler() -> infinite loop
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-23 5:50 AM
Hey guys,
now that the problem with the linker table is finally fixes with FW1.3.0 I have encountered another problem:
If I create a new project in CubeIDE using the standard pin configuration for the WB55 Nucleo board and start debugging after the init sequence the mcu jumps to the Default_handler (startup_....s).
Anybody knows how to fix this?
Best regards,
Philipp
- Labels:
-
STM32CubeIDE
-
STM32WB series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-23 9:08 AM
Quick update:
This could be related to CPU2 boot. This never happens. If the transport layer is enabled the Default_Handler is called.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-24 1:36 AM
Another update:
Did a clean install on WIN10. CubeIDE 1.1.0 and WB Firmware 1.3.0. Can anyone confirm this is working?
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-24 3:29 AM
Flashed BLE_Stack_fw.bin (1.3.1) to the Nucleo board with no problems. Still the minimal running example keeps jumping to the default_handler as soon as the transport layer is enabled. I tried another WB55 board with the same results while the older projects (like examples or FW_WB 1.2.0) are running fine.
I'd really appreciate any help, this is urgend (as it is an actual product development).
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-24 5:30 AM
Ok, so I tracked the source of the interrupt down (at one point I obviously knew my setup routine). If you encounter a similar problem add the following to your stm32wbxx_it.c:
void RTC_WKUP_IRQHandler(void)
{
HW_TS_RTC_Wakeup_Handler();
}
void IPCC_C1_TX_IRQHandler(void)
{
HW_IPCC_Tx_Handler();
}
void IPCC_C1_RX_IRQHandler(void)
{
HW_IPCC_Rx_Handler();
}
Maybe this is helpful to someone.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2019-10-24 6:24 AM
Enabling interrupts without providing a handler will get you into the hardfault handler, yes.
This is a bug in your project. Providing the respective code upfront would have helped.
> I'd really appreciate any help, this is urgend (as it is an actual product development).
This is an open forum with mostly volunteers, not affiliated with ST. Most have a dayjob of their own.
You can't expect others to solve your problems immediately, for free. And neither hold them responsible.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-02 9:18 AM
Thank you PDeng, had the same error with automatic generated code from STM32CubeMX.