cancel
Showing results for 
Search instead for 
Did you mean: 

using Bluetooth module in project.

SSmit.13
Senior

Hi

  We are using the STM32 in a project and want to use a bluetooth module . I see there are many certified modules out there , but if I use any in a project (even though I dont modify the module at all ),  I have to pay for a bluetooth certification. It doesnt make sense using it in a smaller project if a license has to be paid , if I dont put the logo on the brand, do I still have to pay for it?  Im sure many people have come across the same issue

 

Many thanks

Scott

 

1 ACCEPTED SOLUTION

Accepted Solutions

Previously answered:

https://community.st.com/t5/stm32-mcus-wireless/do-we-have-to-pay-for-a-bluetooth-license-if-we-use-the/m-p/57963/highlight/true#M312

As @Peter BENSCH says there, this is nothing to do with ST - it's what the BT SIG defines.

 


@SSmit.13 wrote:

if I dont put the logo on the brand, do I still have to pay for it?


AIUI, you're also not allowed to call it "Bluetooth"

 

Addendum

https://www.bluetooth.com/fee-schedule/

https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/qualification-process-with-no-required-testing/

 

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @SSmit.13 

Can you give more details about your issue. I think your issue is not related to ST is related to BT SIG.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Previously answered:

https://community.st.com/t5/stm32-mcus-wireless/do-we-have-to-pay-for-a-bluetooth-license-if-we-use-the/m-p/57963/highlight/true#M312

As @Peter BENSCH says there, this is nothing to do with ST - it's what the BT SIG defines.

 


@SSmit.13 wrote:

if I dont put the logo on the brand, do I still have to pay for it?


AIUI, you're also not allowed to call it "Bluetooth"

 

Addendum

https://www.bluetooth.com/fee-schedule/

https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/qualification-process-with-no-required-testing/

 

Pavel A.
Evangelist III

Try to ask your favorite AI (Copilot, Chatgpt...) something like "I need pre-certified Bluetooth Low energy (BLE) module that I can build into my product, without having to certify it for Bluetooth".  I don't quote the reply because it contains names of 3rd party products ))

But finally it says: "while the module itself is pre-certified, the final product might still need to go through some form of certification, depending on the regulations in your region". So, depending on your location or market for your product, you need at least to consult with a professional.