cancel
Showing results for 
Search instead for 
Did you mean: 

Unknown aci_gatt_proc_complete_event

DS.4
Senior II

I am getting this event upon sending : ACI_GATT_EXCHANGE_CONFIG

I can't understand why I am getting it. What procedure is complete?

According to AN5270 I should not get it for that command.

0693W00000VOBljQAH.png

1 REPLY 1
Remy ISSALYS
ST Employee

Hello,

According to the description of ACI_GATT_EXCHANGE_CONFIG command in AN5270, the  ACI_GATT_PROC_COMPLETE_EVENT event is also generated to indicate the end of the procedure:

Perform an ATT MTU exchange procedure.

When the ATT MTU exchange procedure is completed, a ACI_ATT_EXCHANGE_MTU_RESP_EVENT event is generated. A ACI_GATT_PROC_COMPLETE_EVENT event is also generated to indicate the end of the procedure.

Indeed in the events generated list, it's missing the ACI_GATT_PROC_COMPLETE_EVENT event.

Best Regards