cancel
Showing results for 
Search instead for 
Did you mean: 

UART not working with LoRaWAN

KCB11
Associate II

Hi, I'm using the LoRaWAN end node example from the stm32cubewl v1.3.0. The board im using is the RAK3172 based on the stm32wle5ccu6 chip. The application i want to build reads data from a modbus using UART and sends it through lorawan. I have assigned UART1 in the platform settings for debugging in lorawan and UART2 for reading from modbus. When I tested both separately the work perfectly. However when I integrate both together, Lorawan still works and uart 1 works properly, however uart2 stops working. I connected a USB to ttl converted to uart2 to see the if it was sending data, it sends data till Lorawan process starts running after that it doesnt send any data. 

I am mostly using the code that is in STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\LoRaWAN\LoRaWAN_End_Node. The only changes that I have made are to write a function to read from modbus in main.c and call that function in lora_app.c just below the line EnvSensors_Read(&sensor_data);

Yet UART doesnt send any data when called from inside the sendTxData() function. Can someone please help.

 

I am attaching the .ioc, lora_app.c and main.c for reference

1 ACCEPTED SOLUTION

Accepted Solutions
KCB11
Associate II

this didnt work but calling MX_USART2_UART_Init() everytime before using uart2 fixed it for me.

View solution in original post

1 REPLY 1
KCB11
Associate II

this didnt work but calling MX_USART2_UART_Init() everytime before using uart2 fixed it for me.