/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "crc.h" #include "app_lorawan.h" #include "usart.h" #include "gpio.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include "sys_app.h" /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ #define TIMEOUT 1000 //UART_HandleTypeDef huart2; /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); /* USER CODE BEGIN PFP */ uint32_t CRC_HardwareBlock(uint16_t Size, const uint8_t *Buffer); uint8_t CheckCRC(uint16_t Size, const uint8_t *Buffer); /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_CRC_Init(); MX_USART2_UART_Init(); MX_LoRaWAN_Init(); /* USER CODE BEGIN 2 */ int response; uint16_t payload[2]; /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { response=GetCTCoilReading(payload); APP_LOG(TS_ON, VLEVEL_M, "CT Read %d\r\n", response); /* USER CODE END WHILE */ MX_LoRaWAN_Process(); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure LSE Drive Capability */ HAL_PWR_EnableBkUpAccess(); __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW); /** Configure the main internal regulator output voltage */ __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); /** Initializes the CPU, AHB and APB buses clocks */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_10; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK3|RCC_CLOCKTYPE_HCLK |RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1 |RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.AHBCLK3Divider = RCC_SYSCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK) { Error_Handler(); } } /* USER CODE BEGIN 4 */ uint32_t CRC_HardwareBlock(uint16_t Size, const uint8_t *Buffer) { CRC->INIT = 0xFFFF; CRC->POL = 0x8005; CRC->CR = 0xE9; while(Size >= 4) // Do as much as we can at 32-bits { CRC->DR = *((uint32_t *)Buffer); Buffer += 4; Size -= 4; } while(Size >= 2) // Perhaps one of these { *((uint16_t *)&CRC->DR) = *((uint16_t *)Buffer); Buffer += 2; Size -= 2; } while(Size--) // Perhaps one of these *((uint8_t *)&CRC->DR) = *Buffer++; return(CRC->DR); // Return final CRC computation } uint8_t CheckCRC(uint16_t Size, const uint8_t *Buffer) { uint32_t recieved_crc=(Buffer[Size+1]<<8|Buffer[Size]); uint32_t calculated_crc=CRC_HardwareBlock(Size, Buffer); if(recieved_crc == calculated_crc){ return 0; } return 1; } int GetCTCoilReading(uint16_t *payload){ uint8_t cmd1[]={0x00, 0x03, 0x00, 0x00, 0x00, 0x06, 0xC4, 0x19}; // uint8_t cmd1[]="HelloWorldTesting\r\n"; uint8_t cmd2[]={0x00, 0x03, 0x01, 0x00, 0x00, 0x01, 0x84, 0x27}; uint8_t cmd3[]={0x00, 0x03, 0x01, 0x10, 0x00, 0x02, 0xC5, 0xE3}; uint8_t rx_buff1[17]; uint8_t rx_buff2[7]; uint8_t rx_buff3[9]; HAL_UART_Transmit(&huart2, cmd1, sizeof(cmd1), TIMEOUT); APP_LOG(TS_ON, VLEVEL_M, "In CT Read func\r\n"); if(HAL_UART_Receive(&huart2, rx_buff1, 17, TIMEOUT)==HAL_OK) //if transfer is successful { if(CheckCRC(sizeof(rx_buff1)-2, rx_buff1)){ return CRC_ERROR; } payload[0]=(rx_buff1[3]<<8|rx_buff1[4]); payload[1]=(rx_buff1[5]<<8|rx_buff1[6]); } else { return READ_TIMEOUT; } HAL_UART_Transmit(&huart2, cmd2, sizeof(cmd2), TIMEOUT); if(HAL_UART_Receive(&huart2, rx_buff2, 7, TIMEOUT)==HAL_OK) //if transfer is successful { if(CheckCRC(sizeof(rx_buff2)-2, rx_buff2)){ return CRC_ERROR; } } else { return READ_TIMEOUT; } HAL_UART_Transmit(&huart2, cmd3, sizeof(cmd3), TIMEOUT); if(HAL_UART_Receive(&huart2, rx_buff3, 9, TIMEOUT)==HAL_OK) //if transfer is successful { if(CheckCRC(sizeof(rx_buff3)-2, rx_buff3)){ return CRC_ERROR; } } else { return READ_TIMEOUT; } return READ_SUCCESS; } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */