2024-11-06 12:53 PM
Hi,
I am using the STM32 Nucleo WBA52CG evaluation board and programming it using Zephyr v3.7.0 and am looking how to set the Tx output power of the BLE radio. Are there any configs available in Zephyr for the same?
If not, alternatively please suggest a way to do this. I want to configure the Tx output power of the radio to +5 dBm.
Thanks, Kaiwalya
Solved! Go to Solution.
2024-11-07 8:15 AM - edited 2024-11-07 10:34 AM
Hello @BKaiwalya
Could you please change :
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 1:42 AM - edited 2024-11-07 2:22 AM
Hello @BKaiwalya and welcome to the ST Community.
I'm checking this internally (throw internal ticket number 195885) and I will be back to you soon with an answer.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 4:43 AM - edited 2024-11-07 4:46 AM
Hello @BKaiwalya
Could you try to use the same implementation of the Zephyr Project zephyrproject-rtos/zephyr: Primary Git Repository for the Zephyr Project. Zephyr is a new generation, scalable, optimized, secure RTOS for multiple hardware architectures. and replace the zephyr/samples/bluetooth/peripheral_hr/src/main.c at main · zephyrproject-rtos/zephyr by the attached main.c file (including a patch).
Please provide feedback as soon as you have tested this application.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 6:33 AM
Hi,
Thanks for providing the quick patch.I tried it and it gives me the following output on console:
Setting PA output level to : 0x0f
Current TX power level in dBm : -10
Is this expected?
However, I would like to set the Tx output power to +5 dBm, what do I need to configure in param here and where can I find the guide for it:
2024-11-07 8:15 AM - edited 2024-11-07 10:34 AM
Hello @BKaiwalya
Could you please change :
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-07 10:09 AM
Hi,
with this I get the following Tx output power:
Current TX power level in dBm : -5
2024-11-07 10:15 AM
Hi,
using
2024-11-07 10:40 AM
The values for each power are available here. You can download this web page and open it to have the annexe table.
I've added this link to my post of solution. And added the necessary senario to my command. If you find that our support is helpful. Please select the original answer as best answer.
ST Community is always here for you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.