2022-07-08 3:09 AM
Hello,
After prototyping with a Nucleo STM32WLJC, I start to use LoRa-E5 board from Seedstudio with a STM32WLE5 MCU.
I want to make a P2P communication, so I'm trying to make a ping pong project on this board.
I tried starting from seeds LoRaWan exemple, from ST pingpong exemple and also from this repo project and .ioc file(https://github.com/danak6jq/Seeed-LoRa-E5).
But It's not working...
After debuging I find out that in SUBGHZSPI_Transmit function, a timout error occured while waiting for TXE flag to be set.
I can't find any others exemples to compare the configuration...
Does anyone have a idea about whats happenning ? Or a tips that can make me move forward ?
Thanks
Hugo
2022-08-23 4:40 AM
Hi! Did you figureout? I have the same behavor.
2022-08-24 11:18 PM
Hi !
I'm not sure about what happened but I tried with another board and it works.
I tried also to change the LoRa E5 on the LoRa e5 mini and It also works.
I think that I make some misstake on my first board while trying to erase the IT firmware.
Hope it helps
Hugo
2022-08-28 9:00 PM
Any update anyone? I'm having similiar issue, timeout waiting for RXNE flag. The transceiver seems to be somehow off.
2022-08-28 11:30 PM
For me, it seems like I messed up the board while I first try to erase the IT firmware...
With a new board, I only connect the LoRa E5 mini to my stmink, I open STM32CubeProgreammer, click on connect and change OB of the read protection from BB to AA . Then I flash or debug my code using STM32Cube IDE.
Check this issue request on github : https://github.com/Seeed-Studio/LoRaWan-E5-Node/issues/10
The same firmware work on the new board but not on the older one that I make serverals change on the OB while discovering the board...
Today I still don't find how to make work my older board...
2022-08-28 11:54 PM
I have a custom project on a custom board in my case, but the problem seems totally same, SUBGHZSPI_Transmit returns timeout. I've broken several chips and feeling hesitant to flash another one.
2022-08-29 8:17 PM
After some googling, I suggest this could be radio being busted due to incorrect power supply handling. Turns out, there is a pitfall.
This might be worth reading: https://community.st.com/s/question/0D53W000011WcYkSAK/smps-danger-the-device-may-be-destroyed
2022-08-29 11:34 PM
Thank you for reply, second device works fine! Firtst one stuck on line:
} while (READ_BIT(SUBGHZSPI->SR, SPI_SR_TXE) != (SPI_SR_TXE));}
Looks like SUBGHZSPI doesn't have domain clock but it enabled.
2023-10-22 6:03 PM
I have two devices that are stuck on this line as well, did you ever solve this on the first device?
2023-10-22 7:24 PM
One of the problems here is that the loop is bound by iterations, not time.
The release version can probably loop quickly, needs to be bounded by TIME, or have a delay so iterations have some expected elapsed time.
Would suggest insuring that SysTick is working and use that, or find TIM you can clock at 1 MHz or so.