SMPS - Danger the device may be destroyed
Hi all,
I read this advertising in the datasheet:
<<
The SMPS needs a clock to be functional. If for any reason this clock stops, the device may
be destroyed.
[...]
Danger: Before enabling the SMPS, the SMPS clock detection must be enabled in the sub-GHz radio SUBGHZ_SMPSC0R.CLKDE.
>>
I only found references to SUBGHZ_SMPSC0R in:
- STM32Cube_FW_WL_V1.0.0\Middlewares\Third_Party\SubGHz_Phy\stm32_radio_driver\radio_driver.h
#define SUBGHZ_SMPSC0R 0x0916
- STM32Cube_FW_WL_V1.0.0\Projects\NUCLEO-WL55JC\Examples\PWR\PWR_SMPS\Src\main.c
Use example
In the Datasheet:
<<
The LDO or SMPS step-down converter operating mode can be configured by one of the
following:
• by the MCU using the SMPSEN setting in PWR control register 5 (PWR_CR5), that
depends upon the MCU system operating mode (Run, Stop, Standby or Shutdown).
• by the sub-GHz radio using SetRegulatorMode() command and the sub-GHz radio
operating mode (Sleep, Calibrate, Standby, Standby with HSE32 or Active).
After any POR and NRST reset, the LDO mode is selected. The SMPS selection has priority
over LDO selection.
>>
I don´t find any reference about "SetRegulatorMode()"
In the Reference Manual:
<<
PWR control register 5 (PWR_CR5) --> Reset value: 0x0000 0000
Bit 15 SMPSEN: SMPS step-down converter enable
This bit enables the SMPS step-down converter.
0: SMPS step-down converter SMPS mode disabled (LDO mode enabled)
1: SMPS step-down converter SMPS mode enabled
Caution: Before enabling the SMPS, the SMPS clock detection must be enabled in the subGHz radio SUBGHZ_SMPSC0R.CLKDE.
Bit 14 RFEOLEN: sub-GHz radio end-of-life detector enable
0: Radio end-of-life detector disabled
1: Radio end-of-life detector enabled
Bits 13:0 Reserved, must be kept at reset value.
>>
In the radio_driver.h code:
<<
/*Sub-GHz radio SMPS control 0 register */
#define SUBGHZ_SMPSC0R 0x0916
[...]
/*Sub-GHz radio SMPS control 2 register */
#define SUBGHZ_SMPSC2R 0x0923
>>
The SUBGHZ_SMPSC2R registers is used by:
static void Radio_SMPS_Set(uint8_t level)
If I use Applications\LoRaWAN\LoRaWAN_End_Node in the Nucleo-WL55JC1
Is SMPS enabled by the LoRa radio Driver?
Do I have to worry about this "device may be destroyed" warning?
Do I have to implement clock detection?
Best Regards
Sergio