2022-03-24 5:58 AM
Hello,
I configure SUBGHZ peripheral to communicate with a RF433MHz module.
The RF433MHz module send preamble and synchronisation word in little-endian fashion (bit 0 first, bit 7 last)
For example, a Sync Word pattern of 0x2D 0xD4 is transmit as 0xB4 0x2B and the preamble of 0b10101010 is received 0b01010101
How can I configure the SUBGHZ peripheral to receive preamble and synchronization word correctly?
Thank you,
Sincerely.
Solved! Go to Solution.
2022-03-24 8:29 AM
It is ok, I have resolved the problem of the preamble, the preamble have 8 bytes length but I should configure 8-bit preamble detection to detect it correctly.
For the synchronisation word I receive it always in little-endian: if my transmitter sends 0x2D 0xD4, I should configure 0xB4 0x2B for SUBGHZ peripheral!
Consequently, I receive data correctly :smiling_face_with_smiling_eyes:
2022-03-24 7:51 AM
Here more precision:
If I send:
Preamble: 1010 1010
Sync word: 0010 1011 (0x2D)
Data: 0111 0101 (0x75)
Bits on air will be: 0101 0101 0100 1101 1110 1010
Because SUBGHZ interface is waiting to 1010… the first bit (the 0) is ignored and I receive:
1010 1010 1001 1011 1101 010 (so the packet will be shifted to left)
So:
received preamble: 1010 1010
received Sync word: 1001 1011 (wrong)
data will be also wrong but just because the shifting.
2022-03-24 8:29 AM
It is ok, I have resolved the problem of the preamble, the preamble have 8 bytes length but I should configure 8-bit preamble detection to detect it correctly.
For the synchronisation word I receive it always in little-endian: if my transmitter sends 0x2D 0xD4, I should configure 0xB4 0x2B for SUBGHZ peripheral!
Consequently, I receive data correctly :smiling_face_with_smiling_eyes: