cancel
Showing results for 
Search instead for 
Did you mean: 

SUBGHZ _ Configure data reception _ little-endian

malarab
Senior II

Hello,

I configure SUBGHZ peripheral to communicate with a RF433MHz module.

The RF433MHz module send preamble and synchronisation word in little-endian fashion (bit 0 first, bit 7 last)

For example, a Sync Word pattern of 0x2D 0xD4 is transmit as  0xB4 0x2B and the preamble of 0b10101010 is received 0b01010101

How can I configure the SUBGHZ peripheral to receive preamble and synchronization word correctly?

Thank you,

Sincerely.

1 ACCEPTED SOLUTION

Accepted Solutions
malarab
Senior II

It is ok, I have resolved the problem of the preamble, the preamble have 8 bytes length but I should configure 8-bit preamble detection to detect it correctly.

For the synchronisation word I receive it always in little-endian: if my transmitter sends 0x2D 0xD4, I should configure 0xB4 0x2B for SUBGHZ peripheral!

Consequently, I receive data correctly :smiling_face_with_smiling_eyes:

View solution in original post

2 REPLIES 2
malarab
Senior II

Here more precision:

If I send:

Preamble: 1010 1010

Sync word: 0010 1011 (0x2D)

Data: 0111 0101 (0x75)

Bits on air will be: 0101 0101 0100 1101 1110 1010

Because SUBGHZ interface is waiting to 1010… the first bit (the 0) is ignored and I receive:

1010 1010 1001 1011 1101 010 (so the packet will be shifted to left)

So:

received preamble: 1010 1010

received Sync word: 1001 1011 (wrong)

data will be also wrong but just because the shifting. 

malarab
Senior II

It is ok, I have resolved the problem of the preamble, the preamble have 8 bytes length but I should configure 8-bit preamble detection to detect it correctly.

For the synchronisation word I receive it always in little-endian: if my transmitter sends 0x2D 0xD4, I should configure 0xB4 0x2B for SUBGHZ peripheral!

Consequently, I receive data correctly :smiling_face_with_smiling_eyes: