2023-06-21 09:31 PM
Is the DevEUI ID also provided in the hardware for stm32wle , in datasheet it is mentioned it is DevEUI compliant. Does it also have a UID64 register from where it can be read?
2023-07-17 07:54 AM
Hello @LGEOR.1 and welcoem to ST Community.
The STM32WLE have an UID64 register from where you can read the DevEUI.
I hope this is helpful for you.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.