2023-07-28 07:39 AM
Hello everyone, I am using 3 STM32WL55JC1. One for base station and the other two's for sensor node. Everything was fine but then I started UART communication between base station and ESP32. I started coding ESP32 so I unplug the usb cables of stm32wl55jc1 (base station) but GND-GND, RX-TX , TX-RX is still plugged between base station and esp32. After a while, I realize my STM32WL55JC1's lora is not working. I can't send anything and I can't receive anything but microcontroller still working. I don't know why it is happening. Any idea ?
2023-07-28 08:16 AM
Hello @AHakk.1 and welcome to ST Community.
I suggest you should check whether the power settings are stable and sufficient for the operation. To do this, you have to compare them before and after unplugging the USB cable.
When your question is answered, please close this topic by choosing "Accept as Solution". This will help other users find that answer faster.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-31 01:05 AM
Okay thank you. I have 3 stm32wl55jc1 module. 2 of them working with out problem as end node or base station. One of them is not working either node or base station. This module's microcontroller works but as I said lora is not working. I don't understand what happened lora part.
2023-07-31 03:09 AM
Hello again
I suggest you to reset them all. This may help to clear any interference that may have occurred.
Best regards.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-31 03:35 AM
Hello again, thanks for reply. I am pressing reset button if thats what you suggest. I can see this when I upload sensor node example.
Sensor start -> ID=01 , RF=868000000MHz , SF=7 , CS=-80dBm
-> 0s134:RF Channel Sensing #1 ... CS: -128dBm , CS time: 10ms
I am uploading same code to my 2 module. One of them sending message but this broken one is not sending.
2023-07-31 03:41 AM - edited 2023-07-31 03:42 AM
Hello again,
They are maybe sending both in the same time using the same channel that's why you can see just one of them. Can you try to stop the one who works fine and take a look if the other is sending fine or not.
Best Regards.
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-07-31 07:01 AM
One of them (broken one) does not send when alone or together but I can see this on serial port.
Sensor start -> ID=01 , RF=868000000MHz , SF=7 , CS=-80dBm
-> 0s134:RF Channel Sensing #1 ... CS: -128dBm , CS time: 10ms
2023-07-31 07:19 AM
Hello again,
Can you erase and flash the code again for the broken one. If you still have the same problem, I suggest you to use the ping pong example to test the broken board.
Best Regards.
Issam
Best Regards.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-22 08:11 AM - edited 2023-08-26 03:51 AM
One of them serves as a base station, and the other two are acting as sensor nodes. Everything was running smoothly until I started implementing UART communication between the base station and an ESP32. While I was coding for the ESP32, I disconnected the USB cables from the STM32WL55JC1 (base station), but I left the GND-GND, RX-TX, and TX-RX connections between the base station and the ESP32 intact.
https://pinterestvideodownloader.io/
2023-08-22 01:29 PM
Hello @harryrex and welcome to ST Community.
I suggest you to do restart to your base station.
Hope this is helpful.
II