2024-01-25 01:10 AM
Hi everyone,
I want to develop a end node module using STM32WL55JC. I have tried to LoRaWAN_End_Node_DualCore example project and the end node has connected to TTN. After that the usart1 enabled and try to send message but i couldnt send message. How can i use peripheral(i2c, uart, adc etc.) with LoRaWAN_End_Node_DualCore/LoRaWAN_End_Node.
2024-01-25 02:26 AM - edited 2024-01-25 02:27 AM
Hello @turen and welcome to the ST Community
I suggest you follow this playlist specially the implementation of the IKS01A3 (video 6) that use I2C to communicate with the example. you can try the same steps and take a look at the changes that acquired on the .c/.h files. Then, you can adapt this method to your specific needs.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-26 06:43 AM
Hi again,
i try to create a lorawan project working on single core. can i use M0plus core for lorawan project and M4 core for general purpose. when i try to create new project, cubemx use both core for lorawan. how can i disable cortex-M4 core shown as below image
2024-01-26 07:40 AM
The LORAWAN middleware need to be activated on both contexts "Cortex-M4 and Cortex-M0+" for Dual core projects.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-29 01:22 AM
I dont want to use IKS01A3 library because Software package not contain all sensors. I want to learn how to use stm32 Peripherals with lorawan end node app and then i will create custom library.
Issue Summary: How to use peripherals(uart, i2c or ADC etc.) with lorawan end node project.
2024-01-29 02:07 AM
Hi,
You don't have to use the IKS01A3. You just have to refer to the video to understand how to use an API (I2C as example) with a LoRawan end node project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.